2017-06-03 7:50 AM
Hello,
I try to install drivers for the above module but the widow says'no mbed microcontrollers found' I can see in the device manager'ST link debug' & 'ST link VPC ctrl' ,
When I connect the STM module to my PC is being recognise somehow and opens an autoplay window that prompts me to open file to view content.
HOWEVER when I try to compile to the module the blinky example , it just downloads a . bin file to my PC. Can you please advise?
EDIT> I understand now that I have to copy the bin to the module directly. What about the device manager? How can I install the drivers?
Thank you
Best Regards
2017-06-03 12:04 PM
The STM32F469I-DISCO ? Not clear what version of Windows you are using.
Installing the ST-LINK Utilities should pull the drivers in, and also allow you to update the ST-LINK firmware to current version.
I'd generally use the utilities to write .BIN and .HEX files to the processor, over the mass-storage controller method.
The ST-LINK drivers should support the MSC and VCP out-of-the-box.
2017-06-03 2:21 PM
Thank you for the reply,
I use windows 7, when I run the update utility it says no ST link device detected.
Mean while when I download the utility it says that is the NUcleo utility but I want to update the Discovery.
Can you please explain me where do I find the utility to write the bin files?
Thank you
2017-06-03 3:38 PM
The utilities are agnostic, it doesn't care if the ST-LINK chip is on a DISCO, NUCLEO, or stand-alone adapter, they ALL function in materially the same way. The mbed variant initially shipped on NUCLEO boards but is now on most of the DISCO boards too.
If the utilities can't find the board it might be open/connected in some other app, or need to be reset so it is in update mode rather than debugger mode.
The utilities allow you to load a .HEX or .BIN, connect via the ST-LINK and program the target STM32 processor.
Tool chains like Keil and IAR integrate ST-LINK support allowing for a direct build and download into the target.
2017-06-05 2:48 AM
Hello,
I have managed to update the firmware but first I installed the USB windows drivers!
Is there a way to again load in the module the preinstalled example interface?
Thank you
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.