2020-01-22 2:45 PM
Hi,
I've made a code that sends the same CAN message but different IDs, I'm using a USB - to - CAN logger to see the communication between these three CANS (1,2,3). I'm running into a problem where the code compiles fine, builds fine, and debugs successfully into the Nucleo board but doesn't transmits/receives any messages through CAN 2 & 3. CAN 1 works fine and receives (works because there's an RX interrupt as well -> LED Blinks) . These are the measures I've taken in trying to figure out what's happening:
-Re-initialized the CANS through the CUBE interface software
-Disconnected each CANL & CANH pin in figuring out one by one which ones were working
-CANS are all the same parameters and matched accordingly to reference, CAN1 works, so I'm just puzzled as to why CAN2,3 are not?? Note: CAN2 is a slave, CAN3 is a master
Given:
-Can bus (120 Ohms terminating bus)
-GND
-Power to each 3x Transciever
-Pins connected accordingly to Tx/Rx of the IC transciever
-CANL/CANHs are connected fine
-Code is attached below
-A JPG is attached below, indicating CAN1's messege is recieved by my logger as well as an interrupt happening through RX of CAN1, although I did enable interrupts for CAN2,3 , they don't work (Physically disconnected the CANL/CANH pins per canbus to pinpoint)
Any help would be greatly appreciated!
Solved! Go to Solution.
2020-01-22 10:39 PM
You should get the Rx running first to set your timing bits correctly to the external dongle you have.
then you can send with TX
Rx
void checkCanRxFifos(void) {
int readCanBytecount;
canTrafficCounter++;
char canFifo1FullFlag = CAN->RF1R & CAN_RF1R_FMP1;
if (canFifo1FullFlag) {
{
readCanBytecount = (CAN->sFIFOMailBox[1].RDTR & 0x0f);
canRxMsgBottomWord[canRxMsgIN] = CAN->sFIFOMailBox[1].RDLR;
canRxMsgTopWord[canRxMsgIN] = CAN->sFIFOMailBox[1].RDHR;
canRxMsgID[canRxMsgIN] = CAN->sFIFOMailBox[1].RIR >> 21;
CAN->RF1R |= CAN_RF1R_RFOM1; // release FIFO
canRxMsgLength[canRxMsgIN] = readCanBytecount;
canRxMsgIN++;
canRxMsgIN &= 0x3F; // 64 entries only
canRxMsgTableEMPTY = false;
if (canRxMsgIN == canRxMsgOUT) canRxMsgTableFULL = true;
}
CAN->IER |= CAN_IER_FMPIE1; // (11) Set FIFO1 message pending IT enable
}
char canFifo0FullFlag = CAN->RF0R & CAN_RF0R_FMP0;
if (canFifo0FullFlag) {
{
readCanBytecount = (CAN->sFIFOMailBox[0].RDTR & 0x0f);
canRxMsgBottomWord[canRxMsgIN] = CAN->sFIFOMailBox[0].RDLR;
canRxMsgTopWord[canRxMsgIN] = CAN->sFIFOMailBox[0].RDHR;
uint32_t canRxmsgID = CAN->sFIFOMailBox[0].RIR >> 21;
CAN->RF0R |= CAN_RF0R_RFOM0; // release FIFO
if(canRxMsgTableFULL) {
canRxMsgTableOverflow = true; // now dump new frame...
}else {
canRxMsgID[canRxMsgIN] = canRxmsgID;
canRxMsgLength[canRxMsgIN] = readCanBytecount; // to signify FIFO0
canRxMsgIN++;
canRxMsgIN &= 0x3F; // 64 entries only
canRxMsgTableEMPTY = false;
if (canRxMsgIN == canRxMsgOUT)
canRxMsgTableFULL = true;
}
// int length;
// length = sprintf(string + length,"%08X, %08X :W",canFifoBuf.d32[0],canFifoBuf.d32[1]);
// for( int i = 0; i < readCanBytecount; i++){
// canRxBuffer[canRxpointerIN++] = canFifoBuf.d8[i];
// canRxpointerIN &= 0xFF;
// if (canRxpointerIN == canRxpointerOUT ) CanRxbufferOverrun = true;
// //length += sprintf(string + length,"%02X, ",canFifoBuf.d8[i]);
// }
// sprintf(string + length -2,"\n\r"); // remove 2 bytes, the last comma and space
}
CAN->IER |= CAN_IER_FMPIE0; // (11) Set FIFO1 message pending IT enable
}
// if (length >0) puts(string);
}TX
void checkCanTxMsgs(void) { // this is modified only to send the very freshest data.
// this is a non-ordered packet transmitter.
//int canMsgCounter =0;
if(!canTxMsgTableEMPTY)
{
//if ((canTxMsgOUT != canTxMsgIN) || canTxMsgTableFULL) // non-ordered packet transmitter
{
if ((CAN->TSR & CAN_TSR_TME0) == CAN_TSR_TME0) // (1)
{
canTrafficCounter++;
canTxMsgOUT = (canTxMsgIN - 1) & 0x3F;
if (showRxCanFrames)
sendCanTxFrametoConsole();
// adjusting to the last saved frame
CAN->sTxMailBox[0].TDTR = canTxMsgLength[canTxMsgOUT]; // (2) length
CAN->sTxMailBox[0].TDLR = canTxMsgBottomWord[canTxMsgOUT]; // (3) 4bytes
CAN->sTxMailBox[0].TDHR = canTxMsgTopWord[canTxMsgOUT]; // (3) 4bytes
CAN->sTxMailBox[0].TIR = ((uint32_t)canTxMsgID[canTxMsgOUT] << 21 | CAN_TI0R_TXRQ); // (4) // send it now if the line is idle
// destroy old data to be sure we only transmit fresh data
// not needed
canTxMsgLength[canTxMsgOUT] = 0;
canTxMsgBottomWord[canTxMsgOUT] = 0;
canTxMsgTopWord[canTxMsgOUT] = 0;
canTxMsgID[canTxMsgOUT++] = 0;
canTxMsgOUT &= 0x3F; // 64 buffer elements
canTxMsgTableFULL = false;
canTxMsgOverrun = false;
}
// if ((canTxMsgOUT != canTxMsgIN) || canTxMsgTableFULL)
// if ((CAN->TSR & CAN_TSR_TME1) == CAN_TSR_TME1) // (1)
// {
// if (showRxCanFrames)
// sendCanTxFrametoConsole();
// CAN->sTxMailBox[1].TDTR = canTxMsgLength[canTxMsgOUT]; // (2) length
// CAN->sTxMailBox[1].TDLR = canTxMsgBottomWord[canTxMsgOUT]; // (3) 4bytes
// CAN->sTxMailBox[1].TDHR = canTxMsgTopWord[canTxMsgOUT]; // (3) 4bytes
// CAN->sTxMailBox[1].TIR = ((uint32_t) canTxMsgID[canTxMsgOUT] << 21 | CAN_TI1R_TXRQ); // (4) // send it now if the line is idle
//
// // destroy old data to be sure we only transmit fresh data
// // not needed
// canTxMsgLength[canTxMsgOUT] = 0;
// canTxMsgBottomWord[canTxMsgOUT] = 0;
// canTxMsgTopWord[canTxMsgOUT] = 0;
// canTxMsgID[canTxMsgOUT++] = 0;
//
// canTxMsgOUT &= 0x3F; // 64 buffer depth
// canTxMsgOverrun = false;
// canTxMsgTableFULL = false;
// //canMsgCounter ++;
// }
// if ((canTxMsgOUT != canTxMsgIN) || canTxMsgTableFULL)
// if ((CAN->TSR & CAN_TSR_TME2) == CAN_TSR_TME2) // (1)
// {
// if (showRxCanFrames)
// sendCanTxFrametoConsole();
// CAN->sTxMailBox[2].TDTR = canTxMsgLength[canTxMsgOUT]; // (2) length
// CAN->sTxMailBox[2].TDLR = canTxMsgBottomWord[canTxMsgOUT]; // (3) 4bytes
// CAN->sTxMailBox[2].TDHR = canTxMsgTopWord[canTxMsgOUT]; // (3) 4bytes
// CAN->sTxMailBox[2].TIR = ((uint32_t) canTxMsgID[canTxMsgOUT] << 21 | CAN_TI2R_TXRQ); // (4) // send it now if the line is idle
//
// // destroy old data to be sure we only transmit fresh data
// // not needed
// canTxMsgLength[canTxMsgOUT] = 0;
// canTxMsgBottomWord[canTxMsgOUT] = 0;
// canTxMsgTopWord[canTxMsgOUT] = 0;
// canTxMsgID[canTxMsgOUT++] = 0;
//
//
// canTxMsgOUT &= 0x3F; // 64 buffer elements
// canTxMsgOverrun = false;
// canTxMsgTableFULL = false;
// //canMsgCounter ++;
// }
if (canTxMsgOUT == canTxMsgIN) canTxMsgTableEMPTY = true;
}
}
}
2020-01-22 3:01 PM
2020-01-22 3:20 PM
2020-01-22 10:39 PM
You should get the Rx running first to set your timing bits correctly to the external dongle you have.
then you can send with TX
Rx
void checkCanRxFifos(void) {
int readCanBytecount;
canTrafficCounter++;
char canFifo1FullFlag = CAN->RF1R & CAN_RF1R_FMP1;
if (canFifo1FullFlag) {
{
readCanBytecount = (CAN->sFIFOMailBox[1].RDTR & 0x0f);
canRxMsgBottomWord[canRxMsgIN] = CAN->sFIFOMailBox[1].RDLR;
canRxMsgTopWord[canRxMsgIN] = CAN->sFIFOMailBox[1].RDHR;
canRxMsgID[canRxMsgIN] = CAN->sFIFOMailBox[1].RIR >> 21;
CAN->RF1R |= CAN_RF1R_RFOM1; // release FIFO
canRxMsgLength[canRxMsgIN] = readCanBytecount;
canRxMsgIN++;
canRxMsgIN &= 0x3F; // 64 entries only
canRxMsgTableEMPTY = false;
if (canRxMsgIN == canRxMsgOUT) canRxMsgTableFULL = true;
}
CAN->IER |= CAN_IER_FMPIE1; // (11) Set FIFO1 message pending IT enable
}
char canFifo0FullFlag = CAN->RF0R & CAN_RF0R_FMP0;
if (canFifo0FullFlag) {
{
readCanBytecount = (CAN->sFIFOMailBox[0].RDTR & 0x0f);
canRxMsgBottomWord[canRxMsgIN] = CAN->sFIFOMailBox[0].RDLR;
canRxMsgTopWord[canRxMsgIN] = CAN->sFIFOMailBox[0].RDHR;
uint32_t canRxmsgID = CAN->sFIFOMailBox[0].RIR >> 21;
CAN->RF0R |= CAN_RF0R_RFOM0; // release FIFO
if(canRxMsgTableFULL) {
canRxMsgTableOverflow = true; // now dump new frame...
}else {
canRxMsgID[canRxMsgIN] = canRxmsgID;
canRxMsgLength[canRxMsgIN] = readCanBytecount; // to signify FIFO0
canRxMsgIN++;
canRxMsgIN &= 0x3F; // 64 entries only
canRxMsgTableEMPTY = false;
if (canRxMsgIN == canRxMsgOUT)
canRxMsgTableFULL = true;
}
// int length;
// length = sprintf(string + length,"%08X, %08X :W",canFifoBuf.d32[0],canFifoBuf.d32[1]);
// for( int i = 0; i < readCanBytecount; i++){
// canRxBuffer[canRxpointerIN++] = canFifoBuf.d8[i];
// canRxpointerIN &= 0xFF;
// if (canRxpointerIN == canRxpointerOUT ) CanRxbufferOverrun = true;
// //length += sprintf(string + length,"%02X, ",canFifoBuf.d8[i]);
// }
// sprintf(string + length -2,"\n\r"); // remove 2 bytes, the last comma and space
}
CAN->IER |= CAN_IER_FMPIE0; // (11) Set FIFO1 message pending IT enable
}
// if (length >0) puts(string);
}TX
void checkCanTxMsgs(void) { // this is modified only to send the very freshest data.
// this is a non-ordered packet transmitter.
//int canMsgCounter =0;
if(!canTxMsgTableEMPTY)
{
//if ((canTxMsgOUT != canTxMsgIN) || canTxMsgTableFULL) // non-ordered packet transmitter
{
if ((CAN->TSR & CAN_TSR_TME0) == CAN_TSR_TME0) // (1)
{
canTrafficCounter++;
canTxMsgOUT = (canTxMsgIN - 1) & 0x3F;
if (showRxCanFrames)
sendCanTxFrametoConsole();
// adjusting to the last saved frame
CAN->sTxMailBox[0].TDTR = canTxMsgLength[canTxMsgOUT]; // (2) length
CAN->sTxMailBox[0].TDLR = canTxMsgBottomWord[canTxMsgOUT]; // (3) 4bytes
CAN->sTxMailBox[0].TDHR = canTxMsgTopWord[canTxMsgOUT]; // (3) 4bytes
CAN->sTxMailBox[0].TIR = ((uint32_t)canTxMsgID[canTxMsgOUT] << 21 | CAN_TI0R_TXRQ); // (4) // send it now if the line is idle
// destroy old data to be sure we only transmit fresh data
// not needed
canTxMsgLength[canTxMsgOUT] = 0;
canTxMsgBottomWord[canTxMsgOUT] = 0;
canTxMsgTopWord[canTxMsgOUT] = 0;
canTxMsgID[canTxMsgOUT++] = 0;
canTxMsgOUT &= 0x3F; // 64 buffer elements
canTxMsgTableFULL = false;
canTxMsgOverrun = false;
}
// if ((canTxMsgOUT != canTxMsgIN) || canTxMsgTableFULL)
// if ((CAN->TSR & CAN_TSR_TME1) == CAN_TSR_TME1) // (1)
// {
// if (showRxCanFrames)
// sendCanTxFrametoConsole();
// CAN->sTxMailBox[1].TDTR = canTxMsgLength[canTxMsgOUT]; // (2) length
// CAN->sTxMailBox[1].TDLR = canTxMsgBottomWord[canTxMsgOUT]; // (3) 4bytes
// CAN->sTxMailBox[1].TDHR = canTxMsgTopWord[canTxMsgOUT]; // (3) 4bytes
// CAN->sTxMailBox[1].TIR = ((uint32_t) canTxMsgID[canTxMsgOUT] << 21 | CAN_TI1R_TXRQ); // (4) // send it now if the line is idle
//
// // destroy old data to be sure we only transmit fresh data
// // not needed
// canTxMsgLength[canTxMsgOUT] = 0;
// canTxMsgBottomWord[canTxMsgOUT] = 0;
// canTxMsgTopWord[canTxMsgOUT] = 0;
// canTxMsgID[canTxMsgOUT++] = 0;
//
// canTxMsgOUT &= 0x3F; // 64 buffer depth
// canTxMsgOverrun = false;
// canTxMsgTableFULL = false;
// //canMsgCounter ++;
// }
// if ((canTxMsgOUT != canTxMsgIN) || canTxMsgTableFULL)
// if ((CAN->TSR & CAN_TSR_TME2) == CAN_TSR_TME2) // (1)
// {
// if (showRxCanFrames)
// sendCanTxFrametoConsole();
// CAN->sTxMailBox[2].TDTR = canTxMsgLength[canTxMsgOUT]; // (2) length
// CAN->sTxMailBox[2].TDLR = canTxMsgBottomWord[canTxMsgOUT]; // (3) 4bytes
// CAN->sTxMailBox[2].TDHR = canTxMsgTopWord[canTxMsgOUT]; // (3) 4bytes
// CAN->sTxMailBox[2].TIR = ((uint32_t) canTxMsgID[canTxMsgOUT] << 21 | CAN_TI2R_TXRQ); // (4) // send it now if the line is idle
//
// // destroy old data to be sure we only transmit fresh data
// // not needed
// canTxMsgLength[canTxMsgOUT] = 0;
// canTxMsgBottomWord[canTxMsgOUT] = 0;
// canTxMsgTopWord[canTxMsgOUT] = 0;
// canTxMsgID[canTxMsgOUT++] = 0;
//
//
// canTxMsgOUT &= 0x3F; // 64 buffer elements
// canTxMsgOverrun = false;
// canTxMsgTableFULL = false;
// //canMsgCounter ++;
// }
if (canTxMsgOUT == canTxMsgIN) canTxMsgTableEMPTY = true;
}
}
}
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.