2020-01-21 9:38 PM
2020-01-22 12:44 AM
The processor reads the first word from the Vector Table at a given address (usually 0x0000'0000, into which in most STM32 usually the FLASH is remapped from 0x0800'0000) and stores it into SP (R14); then it reads the second word and stores it into PC (R15) which means a jump to that address, i.e. program execution starts there.
That's all.
Now toolchains usually supply a method to have the vector table filled by both the interrupt vectors and the execution start address, usually through a startup file, which is often an assembler file (i.e. its name is usually something like startup_stm32XXXX.s). That then also contains the startup code, which initializes the global and static variables required by the C standard, sometimes also performs clocks setup and some other peripherals setup e.g. for external memories, and then jumps to main().
JW
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.