2018-01-29 12:09 PM
Hello, I am using STM32F103 and STM32F301. I need to use the SPI that shares the same pin as SWO. Is it possible to move the SWO to a different pin so I can retain the printf to console functionality for debugging?
Solved! Go to Solution.
2018-01-29 12:29 PM
Only PB3 supported. Use a USART_TX as an alternative.
2018-01-29 12:29 PM
Only PB3 supported. Use a USART_TX as an alternative.
2018-01-29 1:29 PM
Hi Clive, thanks for the info! So I just need to chose a group of pins, such as RX1/TX1, TX2/TX2, RX3/TX3 and get a UART protocol running on those pairs?
2018-01-29 2:58 PM
In the cube, you can hold <cntl> and click the pin to see alternatives, for the SPI port, I mean...
2018-01-29 10:10 PM
You use the cube software, to see the available pins for your requirements.
Did you use the cube before ?
Edit:
before the cube there is the reference material;
PM0214 STM32F3 and STM32F4 Series Cortex®-M4 programming manual.
Also, in the processor data sheet
look for PA9 in the alternate function pin map.
here you can see all the variations of all the pins.
2018-01-30 2:47 AM
SWO =
S
erialW
ireO
utput - as the name suggests, it is output (Tx) only.http://infocenter.arm.com/help/topic/com.arm.doc.ddi0314h/Chdhgebe.html
So there would be no need to reserve an Rx pin for equivalent funcitonality
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.