2016-04-28 7:45 AM
I have a stm32f4-discovery with the stm32f407vg uC on it and I'm trying to program the ADC1 and measure some signals on the port PC7 with it. According to the documentation PC7 hangs on the ADC12_IN15 which I'm interpreting as ADC1 and ADC2 channel 15. I want to use the ADC_DMA example projects from the STD library STM32F4xx_DSP_StdPeriph_Lib_V1.6.1. The signal to the PC7 is provided by a signal generator and it's a square signal with frequency of 5 Hz, Vpp of 3 V and offset of 1.5 V. Then I'm running the following code, which is successfully compiled and uploaded:
#define ADCx ADC1#define ADC_CHANNEL ADC_Channel_15#define ADCx_CLK RCC_APB2Periph_ADC1#define ADCx_CHANNEL_GPIO_CLK RCC_AHB1Periph_GPIOC#define GPIO_PIN GPIO_Pin_5#define GPIO_PORT GPIOC#define DMA_CHANNELx DMA_Channel_1#define DMA_STREAMx DMA1_Stream0#define ADCx_DR_ADDRESS ((uint32_t)0x4001224C)static void ADC_Config(void);/** * @brief Main program * @param None * @retval None */int main(void){ /*!< At this stage the microcontroller clock setting is already configured, this is done through SystemInit() function which is called from startup files (startup_stm32f40_41xxx.s/startup_stm32f427_437xx.s/startup_stm32f429_439xx.s) before to branch to application main. To reconfigure the default setting of SystemInit() function, refer to system_stm32f4xx.c file */ /* ADC configuration */ ADC_Config(); /* Start ADC Software Conversion */ ADC_SoftwareStartConv(ADCx); while (1) { uwADCxConvertedVoltage = uhADCxConvertedValue *3300/0xFFF; }}/** * @brief ADC3 channel07 with DMA configuration * @note This function Configure the ADC peripheral 1) Enable peripheral clocks 2) DMA2_Stream0 channel2 configuration 3) Configure ADC Channel7 pin as analog input 4) Configure ADC3 Channel7 * @param None * @retval None */static void ADC_Config(void){ ADC_InitTypeDef ADC_InitStructure; ADC_CommonInitTypeDef ADC_CommonInitStructure; DMA_InitTypeDef DMA_InitStructure; GPIO_InitTypeDef GPIO_InitStructure; /* Enable ADCx, DMA and GPIO clocks ****************************************/ RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_DMA1, ENABLE); RCC_AHB1PeriphClockCmd(ADCx_CHANNEL_GPIO_CLK, ENABLE); RCC_APB2PeriphClockCmd(ADCx_CLK, ENABLE); /* DMA1 Stream0 channel1 configuration **************************************/ DMA_InitStructure.DMA_Channel = DMA_CHANNELx; DMA_InitStructure.DMA_PeripheralBaseAddr = (uint32_t)ADCx_DR_ADDRESS; DMA_InitStructure.DMA_Memory0BaseAddr = (uint32_t)&uhADCxConvertedValue; DMA_InitStructure.DMA_DIR = DMA_DIR_PeripheralToMemory; DMA_InitStructure.DMA_BufferSize = 1; DMA_InitStructure.DMA_PeripheralInc = DMA_PeripheralInc_Disable; DMA_InitStructure.DMA_MemoryInc = DMA_MemoryInc_Disable; DMA_InitStructure.DMA_PeripheralDataSize = DMA_PeripheralDataSize_HalfWord; DMA_InitStructure.DMA_MemoryDataSize = DMA_MemoryDataSize_HalfWord; DMA_InitStructure.DMA_Mode = DMA_Mode_Circular; DMA_InitStructure.DMA_Priority = DMA_Priority_High; DMA_InitStructure.DMA_FIFOMode = DMA_FIFOMode_Disable; DMA_InitStructure.DMA_FIFOThreshold = DMA_FIFOThreshold_HalfFull; DMA_InitStructure.DMA_MemoryBurst = DMA_MemoryBurst_Single; DMA_InitStructure.DMA_PeripheralBurst = DMA_PeripheralBurst_Single; DMA_Init(DMA_STREAMx, &DMA_InitStructure); DMA_Cmd(DMA_STREAMx, ENABLE); /* Configure ADC1 Channel15 pin as analog input ******************************/ GPIO_InitStructure.GPIO_Pin = GPIO_PIN; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AN; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL ; GPIO_Init(GPIO_PORT, &GPIO_InitStructure); /* ADC Common Init **********************************************************/ ADC_CommonInitStructure.ADC_Mode = ADC_Mode_Independent; ADC_CommonInitStructure.ADC_Prescaler = ADC_Prescaler_Div2; ADC_CommonInitStructure.ADC_DMAAccessMode = ADC_DMAAccessMode_Disabled; ADC_CommonInitStructure.ADC_TwoSamplingDelay = ADC_TwoSamplingDelay_5Cycles; ADC_CommonInit(&ADC_CommonInitStructure); /* ADC1 Init ****************************************************************/ ADC_InitStructure.ADC_Resolution = ADC_Resolution_12b; ADC_InitStructure.ADC_ScanConvMode = DISABLE; ADC_InitStructure.ADC_ContinuousConvMode = ENABLE; ADC_InitStructure.ADC_ExternalTrigConvEdge = ADC_ExternalTrigConvEdge_None; ADC_InitStructure.ADC_ExternalTrigConv = ADC_ExternalTrigConv_T1_CC1; ADC_InitStructure.ADC_DataAlign = ADC_DataAlign_Right; ADC_InitStructure.ADC_NbrOfConversion = 1; ADC_Init(ADCx, &ADC_InitStructure); /* ADC1 regular channel15 configuration **************************************/ ADC_RegularChannelConfig(ADCx, ADC_CHANNEL, 1, ADC_SampleTime_3Cycles); /* Enable DMA request after last transfer (Single-ADC mode) */ ADC_DMARequestAfterLastTransferCmd(ADCx, ENABLE); /* Enable ADC1 DMA */ ADC_DMACmd(ADCx, ENABLE); /* Enable ADC1 */ ADC_Cmd(ADCx, ENABLE);}And I'm expecting to see some data stored in uwADCxConvertedVoltage, or some movement in the ADC1 or the DMA1, but unfortunately there is nothing... :(.What could be wrong?2016-04-28 11:52 AM
What could be wrong?
The ADC uses DMA2, being on APB22016-04-28 11:20 PM
Thank you for your answer. I've changed it to DMA2 and it's still not working, meaning
uwADCxConvertedVoltage is 0 all the time, and no changes in ADC or DMA2 registers. Here is the new code.#define ADCx ADC1#define ADC_CHANNEL ADC_Channel_15#define ADCx_CLK RCC_APB2Periph_ADC1#define ADCx_CHANNEL_GPIO_CLK RCC_AHB1Periph_GPIOC#define GPIO_PIN GPIO_Pin_5#define GPIO_PORT GPIOC#define DMA_CHANNELx DMA_Channel_1#define DMA_STREAMx DMA2_Stream0#define ADCx_DR_ADDRESS ((uint32_t)0x4001224C)static void ADC_Config(void);/** * @brief Main program * @param None * @retval None */int main(void){ /*!< At this stage the microcontroller clock setting is already configured, this is done through SystemInit() function which is called from startup files (startup_stm32f40_41xxx.s/startup_stm32f427_437xx.s/startup_stm32f429_439xx.s) before to branch to application main. To reconfigure the default setting of SystemInit() function, refer to system_stm32f4xx.c file */ /* ADC configuration */ ADC_Config(); /* Start ADC Software Conversion */ ADC_SoftwareStartConv(ADCx); while (1) { uwADCxConvertedVoltage = uhADCxConvertedValue *3300/0xFFF; }}/** * @brief ADC3 channel07 with DMA configuration * @note This function Configure the ADC peripheral 1) Enable peripheral clocks 2) DMA2_Stream0 channel2 configuration 3) Configure ADC Channel7 pin as analog input 4) Configure ADC3 Channel7 * @param None * @retval None */static void ADC_Config(void){ ADC_InitTypeDef ADC_InitStructure; ADC_CommonInitTypeDef ADC_CommonInitStructure; DMA_InitTypeDef DMA_InitStructure; GPIO_InitTypeDef GPIO_InitStructure; /* Enable ADCx, DMA and GPIO clocks ****************************************/ RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_DMA2, ENABLE); RCC_AHB1PeriphClockCmd(ADCx_CHANNEL_GPIO_CLK, ENABLE); RCC_APB2PeriphClockCmd(ADCx_CLK, ENABLE); /* DMA2 Stream0 channel15 configuration **************************************/ DMA_InitStructure.DMA_Channel = DMA_CHANNELx; DMA_InitStructure.DMA_PeripheralBaseAddr = (uint32_t)ADCx_DR_ADDRESS; DMA_InitStructure.DMA_Memory0BaseAddr = (uint32_t)&uhADCxConvertedValue; DMA_InitStructure.DMA_DIR = DMA_DIR_PeripheralToMemory; DMA_InitStructure.DMA_BufferSize = 1; DMA_InitStructure.DMA_PeripheralInc = DMA_PeripheralInc_Disable; DMA_InitStructure.DMA_MemoryInc = DMA_MemoryInc_Disable; DMA_InitStructure.DMA_PeripheralDataSize = DMA_PeripheralDataSize_HalfWord; DMA_InitStructure.DMA_MemoryDataSize = DMA_MemoryDataSize_HalfWord; DMA_InitStructure.DMA_Mode = DMA_Mode_Circular; DMA_InitStructure.DMA_Priority = DMA_Priority_High; DMA_InitStructure.DMA_FIFOMode = DMA_FIFOMode_Disable; DMA_InitStructure.DMA_FIFOThreshold = DMA_FIFOThreshold_HalfFull; DMA_InitStructure.DMA_MemoryBurst = DMA_MemoryBurst_Single; DMA_InitStructure.DMA_PeripheralBurst = DMA_PeripheralBurst_Single; DMA_Init(DMA_STREAMx, &DMA_InitStructure); DMA_Cmd(DMA_STREAMx, ENABLE); /* Configure ADC1 Channel15 pin as analog input ******************************/ GPIO_InitStructure.GPIO_Pin = GPIO_PIN; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AN; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL ; GPIO_Init(GPIO_PORT, &GPIO_InitStructure); /* ADC Common Init **********************************************************/ ADC_CommonInitStructure.ADC_Mode = ADC_Mode_Independent; ADC_CommonInitStructure.ADC_Prescaler = ADC_Prescaler_Div2; ADC_CommonInitStructure.ADC_DMAAccessMode = ADC_DMAAccessMode_Disabled; ADC_CommonInitStructure.ADC_TwoSamplingDelay = ADC_TwoSamplingDelay_5Cycles; ADC_CommonInit(&ADC_CommonInitStructure); /* ADC1 Init ****************************************************************/ ADC_InitStructure.ADC_Resolution = ADC_Resolution_12b; ADC_InitStructure.ADC_ScanConvMode = DISABLE; ADC_InitStructure.ADC_ContinuousConvMode = ENABLE; ADC_InitStructure.ADC_ExternalTrigConvEdge = ADC_ExternalTrigConvEdge_None; ADC_InitStructure.ADC_ExternalTrigConv = ADC_ExternalTrigConv_T1_CC1; ADC_InitStructure.ADC_DataAlign = ADC_DataAlign_Right; ADC_InitStructure.ADC_NbrOfConversion = 1; ADC_Init(ADCx, &ADC_InitStructure); /* ADC1 regular channel15 configuration **************************************/ ADC_RegularChannelConfig(ADCx, ADC_CHANNEL, 1, ADC_SampleTime_3Cycles); /* Enable DMA request after last transfer (Single-ADC mode) */ ADC_DMARequestAfterLastTransferCmd(ADCx, ENABLE); /* Enable ADC1 DMA */ ADC_DMACmd(ADCx, ENABLE); /* Enable ADC1 */ ADC_Cmd(ADCx, ENABLE);}2016-04-30 10:15 AM
ADC1 is on channel 0, not 1.
Cheers, HalWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.