STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

CubeMx STM32F4 feature request implement critical section

Posted on May 01, 2016 at 17:49Hello ST team, I like to see a critical section implementation similar to atmel avrlib ATOMIC_BLOCK implementation. example: ATOMIC_BLOCK(5) {     uint8_t status get_spi_device_info();     if(status == 0) return;     d...

taraben by Senior
  • 711 Views
  • 0 replies
  • 0 kudos

grid connected inverter code problems

Posted on April 30, 2016 at 16:27 hi I have problem with adc sampling and controller calculating at each period of sampling(each sampling time) .I fond this from st,com . I have some questions : 1.what is the meaning of first line exactly an...

Can't make the ADC run on stm32f4-discovery

Posted on April 28, 2016 at 16:45I have a stm32f4-discovery with the stm32f407vg uC on it and I'm trying to program the ADC1 and measure some signals on the port PC7 with it. According to the documentation PC7 hangs on the ADC12_IN15 which I'm inter...

zdravko by Associate II
  • 1721 Views
  • 3 replies
  • 0 kudos

Understanding the difference between USART and SPI controllers

Posted on April 28, 2016 at 15:16Hi, we are surveying microcontrollers for a new product where we need at least 2 SPI interfaces and 2 uart interfaces. All of these 4 interfaces will have to be able to operate concurrently.I have some trouble unders...

audun by Associate
  • 2465 Views
  • 4 replies
  • 0 kudos

STM32/JTAG programming interface doubts

Posted on April 29, 2016 at 01:24STM32 programming interface doubtsHello all.I'm new to ST microcontrollers (STM32 in this case) and JTAG interface. I'm doing the schematic of a project where one of these microcontrollers will be used:- STM32F401RCT...

jeferson by Associate II
  • 7573 Views
  • 8 replies
  • 0 kudos

I2C STM32L053 problem

Posted on April 29, 2016 at 12:19 Hello I have question about i2c. My mcu i2c pin connect to i2c pin evaluation board BU945 My i2c init like this I2C1Handle.Instance = I2C1; I2C1Handle.Init.AddressingMode = I2C_ADDRESSINGMODE_7B...

dree86 by Associate II
  • 940 Views
  • 1 replies
  • 0 kudos

Timer OC problem

Posted on April 19, 2016 at 15:18Hi, I´m using TIM3(output compare mode) in stm32f072 to generate waveform via GPIO. My function principle is: - timer initializing - timer is still running, only is enabled TIM_IT_CC3 a output TIM_CCER_CC3E (BUS_Set_...

STM32F0 custom bootloader

Posted on April 28, 2016 at 07:11Hi, I have made a custom bootloader, but it sometimes freeze when going from bootloader to the actual firmware.  Usually the bootloader should just go to the firmware by doing the following:uint32_t startAddress = *(...

andy2 by Associate II
  • 1423 Views
  • 2 replies
  • 0 kudos

Looking For ST Consultants

Posted on April 01, 2016 at 06:17Hardware. Firmware. iOS.  george@boxunfolded.com  SELF-DESCRIPTIONUser-Centric Full-Stack Embedded Systems Engineer--An Electrical Engineer that knows how to code or a Computer Scientist that knows how to solder.*,**...

gmelcer by Associate
  • 1123 Views
  • 1 replies
  • 0 kudos

How to measure the system core clock on discovery board

Posted on April 29, 2016 at 07:22Hello, I have discovery board , which runs with stm32f407vg MCU. i want to measure the system core clock by bringing it on the gpio or any other means ??Is it doable ? please help me how to do it  #clock #stm32

n.serina by Associate III
  • 1111 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.