2014-07-31 2:29 PM
Hi,
I just received a new prototype with a STM32F215 processor and it is set up to use the SWD interface to initially flash the unit. on the ST-Link/v2 I have connected: pins 3,5 & 10 to gnd (3 & 5 to reduce noise) pin 9 to SWDIO on the processor pin 11 to SWCLK on the processor I have verified the following on the processor: The VDDs are at 3.3v BOOT0 is pulled to ground BOOT1 is floating Vcap_1 & VCAP_2 are at ~ 1.2 v NRST & RESET are high There is a clock on OSC_IN VBAT is connected to 3.3 v In the STM32 ST-LINK Utility: Utility version v3.3.0 USB Driver version v4.3.1.0 ST-Link CLI version V1.9.0 ST-Link version V2.J21.S4 STM32+STM8 Debugger Settings: SWD Coneect Under Reset and tried Normal and tried Hot Plug Enable debug in Low power mode, tried unselected When connecting, I always get: Can not connect to target! Please select ''Connect Under Reset'' .... or If you're trying to connect to an STM32W1xx ... I verified that there seems to be activity on both the SWDIO & SWCLK lines when attempting to connect. Any hints as to what further to check? Thanks for any help! Vance #stm32f2xx-swd-st-link2014-07-31 2:46 PM
nope, Should be pin 7 and 9. Also connect Vcc (3.3V)
2014-07-31 4:10 PM
Thanks for the response!
Actually, it was pins 7 & 9. Sorry for the typo. I had thought the VCC connection was optional. That is going to be difficult. Very small board with all tiny parts. I'll see what I can do and report back tomorrow. Vance2014-08-01 5:51 AM
I made the connection between Vcc and pin 1 of the ST-Link/v2. Still no joy.
any other ideas? Vance2014-08-01 7:22 AM
Voltages suggest the part orientation is correct.
Sure you don't have SWDIO/SWCLK switched around, or connected to the wrong pins on the IC? Time to dig into the schematic. Can you pull BOOT0 High and check for USART1 (PA9/PA10) connectivity to the System Loader? ie RealTerm at 9600 8E1, sending 0x7F, seeing 0x79 response? I perhaps would have wired up SWO and NRST, and used a standard header connector. VCC is semi-optional depending on if the JTAG/SWD pod has line drivers. Bonding pin 1 & 2 of the 20-pin JTAG header should be sufficient to resolve that. NRST should not be driven high, or attached to VDD directly.2014-08-01 7:57 AM
I'm very embarrassed to say, during one of my soldering events, I ended up connecting the the connector to the prototype upside down :(
I do have communications now! As a follow up, Vcc apparently does need to be connected to the ST-Link/v2. Thank you very much for your help! VanceWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.