2024-05-01 3:49 AM - last edited on 2024-05-01 11:20 AM by mƎALLEm
Hello all,
I am using the CAN protocol to read and write data from the Flash memory of one STM32F446ZET6 board to the Flash memory of another STM32F446ZET6 board.
I have tried multiple baud rates. All working properly. However, I notice a 25 ms delay between every CAN frame, regardless of the baud rate.
Is this a default setting and/or is there a way to change this time delay?
Thanks!
Solved! Go to Solution.
2024-05-01 11:19 AM
Hello,
CAN peripheral embedded on STM32 is inline with the CAN protocol standard specified by ISO11898.
So it could be a delay introduced by the APIs overhead or some delay inserted in your code.
2024-05-01 11:19 AM
Hello,
CAN peripheral embedded on STM32 is inline with the CAN protocol standard specified by ISO11898.
So it could be a delay introduced by the APIs overhead or some delay inserted in your code.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.