2020-08-31 8:13 PM
We have built a respirator prototype using a pic microcontroller, which has been tested by doctors and they are satisfied with the results, now we wanted to manufacture the product in a large scale and before that it needs to be certified for IEC 60601. So my question is can I use STM32F103C8 in the product and does it satisfy IEC60601 criteria?
2020-09-01 1:20 AM
This is a primarily user-driven forum, with casual ST presence. You need to ask this question ST directly, through web support form, or through FAE.
JW
2020-09-01 2:01 AM
A first indicator would be the datasheet / reference manual.
Those documents usually contain a disclaimer describing applications the device is not fit for. Like medical applications.
Usually at the very end - at least the TI documents I vividly remember did so.
As Jan suggested, approach ST directly.
2020-09-01 5:27 AM
Thank you both for your quick replies. I have asked the question to the ST directly and awiating their reply.
@Ozone before posting the question I read the description of STM32F103 in their portfolio and datasheet as well, which states that these microcontrollers can be used in medical devices but I could not find any supporting documents.
2020-09-01 6:44 AM
I'm not an expert in this field, but there are several classes.
Many MCU datasheets explicitly state the devices are not appropriate for failsafe devices, e.g. life support.
Something like a blood pressure mesurment device is uncritical in this regard.
2020-09-01 6:58 AM
I'm not a lawyer : Liability and testing, evaluation, certification burden entirely on YOU
"Unless Seller’s Products are expressly designated in the applicable Product Specifications as having been specifically designed for use in: (a) safety critical applications such as life supporting devices or systems; (b) aeronautic or aerospace applications; and/or (c) automotive applications or environments (such as, by way of example, Products designated as “Automotive Grade�? and used in association with a vehicle propelled by a self-contained motor, engine or the like, such as, without limitation, cars, trucks, motorcycles, electric cars, e-bikes and other transportation devices, or in an automotive environment, such as applications for active and passive safety, infotainment, telematics, vehicle body and convenience, electric car charging, insurance black boxes and the like), Buyer’s use of Seller’s Products in such applications contemplated by clauses (a), (b) and/or (c) above shall be at Buyer's sole risk, even if Seller is aware of or has been informed in writing of such usage."
"Disclaimer for critical applications : Product(s) indicated in this presentation are sold under ST terms and conditions and they are not designed, intended or authorized for use as a critical component in life support systems, or any FDA Class 3 medical devices or medical devices with a similar or equivalent classification in a foreign jurisdiction, or any devices intended for implantation in the human body. Contact ST Sales Offices for any further details. "
2021-08-12 12:46 AM
Those documents generally include a disclaimer describing packages the device isn't always healthy for. Like clinical packages here. Usually at the very cease - at the least the TI files I vividly keep in mind did so.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.