2016-08-19 6:14 AM
Hello,
for example: there are stand alone function in program memory,
it doesn't include another function(s), it is not nested, I want to move to sram and to run it there.void MyFunc(void) // in program memory
{
....
}
is it possible? if yes, how can I move and use it? Please can you give me a short sample?
2016-08-19 6:27 AM
Yes, although doing math can call helper/library functions.
IAR has a ''ramfunc'' option. Other tool chains have attributes or pragmas to direct code into specific segments/sections, which can include RAM. One can also memcpy() the function code and literal pool into another location, and then transfer control via a function pointer. Observe how qsort() works. This is a topic I've covered here before. Please review other threads.int TestFunc(void)
{
return(123);
}
#define FUNC_SIZE 64
typedef int (*pFunction)(void);
int RamFunc(void)
{
uint8_t Buffer[FUNC_SIZE];
pFunction RunFunc;
memcpy(Buffer, (void *)((uint32_t)&TestFunc & ~1), FUNC_SIZE); // Copy code
RunFunc = (pFunction)&Buffer[1]; // +1 for Thumb code
return(RunFunc()); // sourcer32@gmail.com
}
2016-08-19 6:58 AM
If you are using a GCC based toolchain just add a small attribute to your function definition and that's all:
void EXTI9_5_IRQHandler(void); becomes void EXTI9_5_IRQHandler(void) __attribute__((section (''.data''))); where .data is your data section (look in your linker *.ld files).2016-08-19 1:30 PM
Thanks a lot for replies
Dear clive1, Likewise for nested functions, Can I use as follows? There are 3 functions but they are nested, Can I move them to sram in program memory while cpu is working, and run them ?typedef
void
(*pFuncP1_t)(u8);
typedef
u8 (*pFuncP2_t)(u32, u32);
typedef
void
(*pFuncP3_t)(u8, u32, u32);
typedef
struct
{
u8 Fonc1_Buf[FONC1_BUF_SIZE];
u8 Fonc2_Buf[FONC2_BUF_SIZE];
u8 Fonc3_Buf[FONC3_BUF_SIZE];
pFuncP1_t pFoncP1;
pFuncP2_t pFoncP2;
pFuncP3_t pFoncP3;
}FoncPtrs_t;
FoncPtrs_t FoncPtrs;
void
Fonc1(u8){
...
}
void
Fonc2(u32, u32){
...
Fonc1(u8);
}
void
Fonc3(u8, u32, u32){
...
Fonc2(u32, u32);
}
// in program
memcpy
(FoncPtrs.Fonc1_Buf, (
void
*)((uint32_t)&Fonc1 & ~1), FONC1_BUF_SIZE);
// func1 copy
FoncPtrs.pFoncP1 = (pFuncP1_t)&FoncPtrs.Fonc1_Buf[1];
memcpy
(FoncPtrs.Fonc2_Buf, (
void
*)((uint32_t)&Fonc2 & ~1), FONC2_BUF_SIZE);
// func2 copy
FoncPtrs.pFoncP2 = (pFuncP1_t)&FoncPtrs.Fonc2_Buf[1];
memcpy
(FoncPtrs.Fonc3_Buf, (
void
*)((uint32_t)&Fonc3 & ~1), FONC3_BUF_SIZE);
// func3 copy
FoncPtrs.pFoncP3 = (pFuncP1_t)&FoncPtrs.Fonc3_Buf[1];
FoncPtrs.pFoncP3();
2016-08-19 1:39 PM
As presented that isn't going to work.
You would be better managing the functions into a RAM section using the Scatter File for the linker.2016-08-19 1:57 PM
Thanks,
in fact, I'm using the same way now (into sram section using the scatter file for bootloader). I'm trying to know this is possible.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.