2018-04-11 5:03 AM
Hi,
I Have a project that can be populated with or without RTC and a battery. Can I leave the VBAT pin unconnected when building PCBs without the battery?
I'm using an STM32F072.
#stm32f0 #stm32 #vbat2018-04-11 8:53 AM
If no battery, both RM0091 and AN4080 recommend to connect it to VDD.
JW
2018-04-11 1:08 PM
Well, yes. You're right. But I was hoping I would not need extra components when I don't mount the battery. Or what if I do mount the battery-holder, but the user forgets to replace the battery when it's empty? That creates a very similar situation as what I have now: Simply a floating VBAT.
I just checked the 'decoupling your STM32F0xx' section in the datasheet. No capacitor on VBAT. And then RM0091 says to install a capacitor when connecting to VDD...
2018-04-11 2:28 PM
I guess you can leave it unconnected as long as you don't use the RTC and other VBAT-related features.
Note that I am not ST so do this on your own risk.
JW
2018-04-11 3:12 PM
use a jumper or solder blob under the battery itself.
if the battery is not installed, you must solder the blob , shorting out the Vbat to VDD
2018-04-11 5:30 PM
Hello,
Capacitor between VBAT pin and ground is not mandatory. If you don't plan to use backup domain, please simply connect VBAT to VDD.
Regards
Szymon
2018-04-11 6:03 PM
A capacitor to ground on the VBAT pin is usually detrimental to the battery life
Not recommended unless you use a high quality poly cap.
2018-04-19 12:32 AM
Why does a capacitor drain the battery? Why would a better cap not do this? You're thinking about leakage current? I don't think of ceramic caps as 'leaky'. I'll see if I can measure the leakage of the 100nF 50V ceramic 0805 capacitors that I have.
2018-04-19 6:15 PM
If you are using a normal Coin Type cell,
I found the basic 0.1uF bypass cap,
reduced the voltage on the battery below 3V within a month.
2018-04-21 9:22 AM
I measured the leakage of my standard 100nF 50V capacitor. It is about 0.1 nA at 10V and about 1nA at 50V.
A 200mAh coin cell would be depleted by such a current after about 63 years.....
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.