2023-05-08 6:24 AM
Hello! I have an STM32L496ZG development board. CAN communication used to work earlier. Once after the recent update of Cube IDE , CAN communication doesn't seem to work. Is anyone facing the same issue?
2023-05-08 11:07 AM
Hello @PO.3 ,
Please share as more details as possible to help you solve your issue.
Which firmware version are you using? You can share a screenshot, or your code.
Localize where the code hangs/stop, when the problem occurs.
Imen
2023-05-08 11:40 AM
Which board are you talking about? The NUCLEO-L496ZG ?
Perhaps go into a bit more detail about you test setup, what you're doing, and your test process.
Try going back to a version that works in your sand-box, and then perhaps diff the related code / library.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.