2026-03-16 8:12 AM - last edited on 2026-03-16 8:19 AM by Andrew Neil
Hello,
I’ve recently started using ST products and the IDE with CubeMX, which is why I’m asking for your help. I’ve just begun developing a communication system using a Nucleo H743ZI2; my goal is to set up a UART and a CAN bus.
The UART is done; I used DMA access to optimize it. However, when I try to enable the CAN bus in Cube MX, I run into a problem with the clock configuration related to the bus.
When I use the “Resolve Clock Issues” function, I get the error: “Cannot find a solution for some constraints.”
Does anyone have any ideas to help me solve this problem?
Thank you in advance, and have a great day,
Solved! Go to Solution.
2026-03-17 6:30 AM
@AmGo wrote:
Is it the clock speed generated by my ST-Link ?
Yes. By selecting Bypass mode, the clock source arrives to OSC_IN pin to feed the RCC which is generated by ST-LINK.
2026-03-17 6:32 AM
Oh, right, that’s exactly what I did. I chose 64 MHz for convenience. It’s not a specific requirement for my project.
Thank you very much for your help.
Have a nice day !
2026-03-17 6:37 AM - edited 2026-03-17 6:37 AM
Ok good.
So please accept as solution the post that answered your original question (asked in your first post).
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.