2019-02-12 1:25 PM
I am porting a code base that used to work well on the STM32F103 series.
The problem I have with the STM32F302VE seems to be related to the CAN FIFO's. What works:
1) CAN registers are working correctly
2) Initialization is executed normally
3) Receive interrupts are triggered when frames are on the bus
The problems I have are:
1) Can't read anything meaningful from the receive FIFO (RX data is all 0x00)
2) Attempt to transmit create a Hard Fault Error when the mailbox is written to
It looks like the FIFO are not enabled or not clocked. I cannot see anything specific to the CAN FIFO's beyond the enable and clock bit for the whole CAN subsystem.
Any idea?
2019-02-12 3:05 PM
The TX issue has been resolved. In the new CAN API:
HAL_CAN_AddTxMessage(CAN_HandleTypeDef *hcan, CAN_TxHeaderTypeDef *pHeader, uint8_t aData[], uint32_t *pTxMailbox)
pTxMailbox is (obviously) a pointer. I was passing a FIFO number.
When getting a hardfault, it is very useful to do:
*(uint8_t *)0xE000E008 |= (2);
This sets the Auxiliary Control Register to disable the write buffer and allows you to detect where the fault is happening.
2019-02-12 5:24 PM
The receive issue also went away when forcing NORMAL mode (as opposed to SILENT). It seems that the simulator used for this development behave differently at different time.
Sorry for the false alarm.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.