2019-02-11 1:07 AM
I have developed my application in Nucleo-L152RE board by using Atollic Truestudio. Now, I want it to migrate to STM32L462CE MCU. So, how I do that in a quick way by using Atollic Studio? Can you provide some quick steps and settings which I have to change in Atollic studio for doing this stuff?.
2019-02-12 5:55 AM
Hello @Community member_SLS (System Level Solution) ,
I recommend you to follow this application note "AN4612 Application note Migrating from STM32L1 Series to STM32L4 Series and STM32L4+ Series microcontrollers" which helps you to migrate from STM32L1 Series to STM32L4 Series.
You can take this Application Note as reference to determine differences between the two series with give attention to pinout, peripherals and system clock...
The advantage of HAL library is that functions' names are the same for all series, so the migration from one device to another is not so complicated.
You may also start from the template project in the STM32CubeL1 package and then add your own modifications (new functions, new files)...
Maybe this video (migration using Keil) helps you to understand the principle of migration: https://st-videos.s3.amazonaws.com/gettindstartedsmt32cubefinal.mp4
Kind Regards,
Imen
2019-02-12 6:18 AM
How easy this is depends on how well your code is abstracted.
I'd suggest creating a small shell project for the new target, get the clock, pins and USARTs up first, and then merge sections of code across, pulling and refactoring the peripheral support as you go.
2019-02-12 8:26 PM
Thanks for your valuable help. I have successfully migrate my application from STM32L1 to STM32L4.
2019-02-12 8:31 PM
Hello @Imen DAHMEN ,
Thanks for you help..!!!
I have migrate my application all modules has worked fine except flash and there is one issue on writing the data into STM32L462CE flash memory.
I have checked and found that if we want to store data into flash memory, we have to store in 8 byte(double word) so, here my requirement is to store data byte by byte which is stored in char array. So, how can I achieve this? can you please help me on this.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.