2018-02-21 9:46 AM
Wrong interrupt name, doesn't match macro, missing DMA_Tx handler
STM32Cube_FW_F7_V1.9.0\Projects\STM32F769I-Discovery\Applications\Display\LCD_PicturesFromSDCard\Src\stm32f7xx_it.c (and .h)
...
/**
* @brief Handles SDMMC1 DMA Rx transfer interrupt request. * @retval None */void BSP_SDMMC1_DMA_Rx_IRQHandler(void){ HAL_DMA_IRQHandler(uSdHandle.hdmarx);}/**
* @brief Handles SD1 card interrupt request. * @retval None */void BSP_SDMMC1_IRQHandler(void){ HAL_SD_IRQHandler(&uSdHandle);}...
Correct defines here, using SDMMC2
STM32Cube_FW_F7_V1.9.0\Drivers\BSP\STM32F769I-Discovery\stm32f769i_discovery_sd.h
...
/* DMA definitions for SD DMA transfer */
#define __DMAx_TxRx_CLK_ENABLE __HAL_RCC_DMA2_CLK_ENABLE#define SD_DMAx_Tx_CHANNEL DMA_CHANNEL_11#define SD_DMAx_Rx_CHANNEL DMA_CHANNEL_11#define SD_DMAx_Tx_STREAM DMA2_Stream5#define SD_DMAx_Rx_STREAM DMA2_Stream0#define SD_DMAx_Tx_IRQn DMA2_Stream5_IRQn#define SD_DMAx_Rx_IRQn DMA2_Stream0_IRQn#define BSP_SDMMC_IRQHandler SDMMC2_IRQHandler#define BSP_SDMMC_DMA_Tx_IRQHandler DMA2_Stream5_IRQHandler#define BSP_SDMMC_DMA_Rx_IRQHandler DMA2_Stream0_IRQHandler#define SD_DetectIRQHandler() HAL_GPIO_EXTI_IRQHandler(SD_DETECT_PIN)...
2018-02-26 6:25 AM
Hello
Turvey.Clive.002
Thank you for posting this bug and bringingit to our attention..
I raised this issue to our development team for fix.
Best Regards,
Imen
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.