2018-02-25 9:11 AM
Hi. I need to start to use the sx1276 for LoRa implementation.
I looked that there is a demoboard that support mbed but I think it is not good for me because I can't use mbed libraries and I need to implement LoRa with St and another type of microcontroller.Could someone suggest to me how to start?I'm a beginner in LoRa and in radio applications in general.2018-02-25 9:34 AM
The LRWAN software is a good place to start
http://www.st.com/en/embedded-software/i-cube-lrwan.html
For the SX1276 either the LoRa Discovery board with the Murata module, or the SX1276 Shield (supported in above code trees)
http://www.st.com/en/evaluation-tools/b-l072z-lrwan1.html
https://os.mbed.com/components/SX1276MB1xAS/
https://community.st.com/community/stm32-community/blog/2017/04/05/lora-discovery-kit
2018-02-25 10:42 AM
I would also suggest that you start with
http://www.st.com/en/evaluation-tools/b-l072z-lrwan1.html
and
http://www.st.com/en/embedded-software/i-cube-lrwan.html
Search this forum for recent discussions on the above.
I can't use mbedWhy not?
I need (sic) to implement LoRa with St and another type of microcontroller.
Not quit sure what you mean by that?
Clearly, this is not the place to discuss other makes of microcontroller!
I'm a beginner in LoRa
Start here:
https://www.lora-alliance.org/
In particular:
https://www.lora-alliance.org/what-is-lora
And, of course, use google; LoRa is quite a 'Hot Topic' at the moment - there are lots of tutorials & examples on the interwebs ...
2018-02-25 12:09 PM
Many thanks.
I think I will buy this
https://www.digikey.it/product-detail/it/semtech-corporation/SX1276MB1MAS/SX1276MB1MAS-ND/5015648
and I will try to implement the protocol explained here
https://www.semtech.com/uploads/documents/sx1276.pdf
because I need to learn how to use LoRa and I need to implement it in both St and Renesas microcontrollers.
I hope it will be not so hard.
2018-02-25 12:13 PM
>>Not quit sure what you mean by that? Clearly, this is not the place to discuss other makes of microcontroller!
The supposition here would be that the LoRa side is partitioned into an STM32 which slaves to a much faster and complex host system, be it a Broadcom, Marvell or Rockchip, etc. running Linux or whatever. I'm not disinclined to tackle systems level integration issues, it is not like the bulk of us work for ST, or have the luxury of working only with Brand X products.
2018-02-25 12:32 PM
I should have said 'recommend' rather than 'discuss'.
2018-02-25 11:15 PM
HC-12 is a cheap long range transmitter receiver. And easy to use. If high power 433MHz =LORA is legal in your country, then HC-12 should be too.
2018-02-26 2:54 AM
Please provide a link to the manufacturer documentation for this 'HC-12'.
I found this:
http://trainelectronics.com/Arduino/HC-12-Serial_Radio/images/HC-12%20v2.3A.pdf
It says,
The HC-12 module uses a Silicon Labs Si4463 to provide RF communications
That is not a LoRa chip:
https://www.silabs.com/documents/public/data-sheets/Si4464-63-61-60.pdf
2018-02-26 5:53 AM
The HC-12 seems like a more obfuscated solution, attaching the STM32 directly to the SX1276 avoids having the STM8 in the way. SiLabs has a newer EZR32 solution which integrates a radio + CM3/4, which replaces the Si1000 8051 based combo, and I'd expect ST to have an integrated solution for LoRa in the future.
The USI and Murata modules integrating SX127x and STM32L0xx parts are pretty cheap and significantly more powerful, to the point of removing a MPU from most solutions.
Also the Semtech LoRa radios work significantly better than SiLabs EZR ones in my experience.
2018-02-26 5:59 AM
Clive One wrote:
I'd expect ST to have an integrated solution for LoRa in the future.
There have been rumours ...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.