2016-08-21 10:24 PM
Hello,
I am use STM32Cube ver. 4.16 and STM32F3xx HAL Driver version number V1.3.0.When using HAL_UART_Receive_IT , during more than once unless you remove a communication cable: the program enters an IT IRQ infinite loop
During more than once unless you remove a communication cable
During more than once unless you remove a communication cable
2016-08-22 2:45 AM
Hi yildirim.yi_it,
What kind of error you get then ? Is it overrun error ? Since you have generated the code using CubeMx 4.16 , may you share you .ioc file. -Hannibal-2016-08-22 4:45 AM
Communication cable to plug and unplug several times , it IRQ endless loop.
Yes, errorcode = 8 Overrun. Attach File .iocCommunication cable to plug and unplug several times , it IRQ endless loop.
________________ Attachments : USART1_F303.ioc : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006Htcv&d=%2Fa%2F0X0000000aS8%2FqB9kUWFE.cCNHXxRe1aIct.KIrxwwOJ2MJ6DxwseZVs&asPdf=false2016-09-16 6:11 AM
Hi
yildirim.yi_it
,It seems you have an overrun error due to pending interrupt.
In order to clear the pending interrupts we provide a specific macros in stm32f4xx_hal_uart.h file that can be used directly by the application (when needed).
Please refer to the Exported macro section in stm32f4xx_hal_uart.h file. The specific macro to clear the overrun pending interrupt is
__HAL_UART_CLEAR_OREFLAG()
Thus you can perform this to avoid overrun issue:
__HAL_UART_CLEAR_OREFLAG(…)
HAL_UART_Receive_IT(…)
-Hannibal-
Communication cable to plug and unplug several times , it IRQ endless loop.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.