2017-03-31 11:00 PM
This code snippet is generated by STMCubeMx 4.6.0 and STM32Cube FW_F1 V1.4.0 for STM32F107
964 uint32_t HAL_RCC_GetSysClockFreq(void)
965 { 966 #if defined(RCC_CFGR2_PREDIV1SRC) 967 const uint8_t aPLLMULFactorTable[12] = {0, 0, 4, 5, 6, 7, 8, 9, 0, 0, 0, 13}; 968 const uint8_t aPredivFactorTable[16] = { 1, 2, 3, 4, 5, 6, 7, 8, 9,10, 11, 12, 13, 14, 15, 16}; 969 #else 970 const uint8_t aPLLMULFactorTable[16] = { 2, 3, 4, 5, 6, 7, 8, 9, 10, 11, 12, 13, 14, 15, 16, 16}; 971 #if defined(RCC_CFGR2_PREDIV1) 972 const uint8_t aPredivFactorTable[16] = { 1, 2, 3, 4, 5, 6, 7, 8, 9,10, 11, 12, 13, 14, 15, 16}; 973 #else 974 const uint8_t aPredivFactorTable[2] = { 1, 2}; 975 #endif /*RCC_CFGR2_PREDIV1*/In my setup, I have SYSCLK from PLLCLK which is generated from HSI. When PLLMUL is set to 6.5,
HAL_RCC_GetSysClockFreq() will try to access the 13th (0x1101) element which is outside the array. Plus where is 13 from?
I am working around this problem by setting PLLMUL to 9 in STMCubeMx.
Solved! Go to Solution.
2017-04-03 3:57 AM
Hi
Li.Hongliang
,I confirmed theHAL issueon the aPLLMULFactorTable, inside
STM32CubeF1 V1.4.0
(stm32f1xx_hal_rcc.c and stm32f1xx_hal_rcc_ex.c)which should be :
const uint8_t aPLLMULFactorTable[14] = {0, 0, 4, 5, 6, 7, 8, 9, 0, 0, 0,
0, 0,
13};This issue is already reported internally and will be fixed in the coming version.
Imen
2017-04-02 9:21 AM
Hi
Li.Hongliang
,You should use the CubeMx version 4.20 as contains enhancements and bug fixes.
I will check your reported issue and come back to you.
Imen
2017-04-03 3:57 AM
Hi
Li.Hongliang
,I confirmed theHAL issueon the aPLLMULFactorTable, inside
STM32CubeF1 V1.4.0
(stm32f1xx_hal_rcc.c and stm32f1xx_hal_rcc_ex.c)which should be :
const uint8_t aPLLMULFactorTable[14] = {0, 0, 4, 5, 6, 7, 8, 9, 0, 0, 0,
0, 0,
13};This issue is already reported internally and will be fixed in the coming version.
Imen
2017-04-03 9:30 AM
Thanks Imen. Nice work!
2018-12-15 8:21 PM
I can confirm that the problem still exists in STM32F1 version 1.7.0 In particular, at line 1128 in HAL_RCC_GetSysClockFreq there is an if statement
if ((tmpreg & RCC_CFGR_PLLSRC) != RCC_PLLSOURCE_HSI_DIV2)
If this evaluates to false - that is if PLL2Mul is not the input to the PLL and the else path is taken - we bypass this code which successfully deals with a PLL mult of 6.5
/* If PLLMUL was set to 13 means that it was to cover the case PLLMUL 6.5 (avoid using float) */
/* In this case need to divide pllclk by 2 */
if (pllmul == aPLLMULFactorTable[(uint32_t)(RCC_CFGR_PLLMULL6_5) >> RCC_CFGR_PLLMULL_Pos])
{
pllclk = pllclk / 2; // MY COMMENT: <-------------- This fixes the 6.5 PLL option
}
Instead all we execute is
else
{
/* HSI used as PLL clock source : PLLCLK = HSI/2 * PLLMUL */
pllclk = (uint32_t)((HSI_VALUE >> 1) * pllmul); // MY COMMENT: We divide by 2 here to take into account Prediv1
}
sysclockfreq = pllclk; // MY COMMENT: <------------- no fix for the pll 6.5 option
break;
}
leaving the clock frequency off by a factor of 2 if pllmul = 0x0D
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.