2015-03-25 5:18 AM
Hi,
I think there is a bug in the HAL layer of ST. (version 1.1.0) My code is very simple: I initialize two GPIO (PB4 and PB5) in Interrupt.GPIO_InitTypeDef GPIO_InitStruct;
// Configure the Port
GPIO_TO_CHECK_1_CLK_ENABLE();
GPIO_TO_CHECK_2_CLK_ENABLE();
GPIO_InitStruct.Mode = GPIO_MODE_IT_RISING;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FAST;
GPIO_InitStruct.Pin = GPIO_TO_CHECK_1_PIN;
HAL_GPIO_Init(GPIO_TO_CHECK_1_PORT, &GPIO_InitStruct);
GPIO_InitStruct.Pin = GPIO_TO_CHECK_2_PIN;
HAL_GPIO_Init(GPIO_TO_CHECK_2_PORT, &GPIO_InitStruct);
// Enable and set Button EXTI Interrupt to the priority 0x03
NVIC_SetPriority((IRQn_Type)GPIO_TO_CHECK_1_EXTI_IRQn, 0x03);
HAL_NVIC_EnableIRQ((IRQn_Type)GPIO_TO_CHECK_1_EXTI_IRQn);
NVIC_SetPriority((IRQn_Type)GPIO_TO_CHECK_2_EXTI_IRQn, 0x03);
HAL_NVIC_EnableIRQ((IRQn_Type)GPIO_TO_CHECK_2_EXTI_IRQn);
Then I code the IRQ handler. PB4 and PB5 are on the same IRQ vector :
void EXTI4_15_IRQHandler(void)
{
if(__HAL_GPIO_EXTI_GET_IT(GPIO_TO_CHECK_2_PIN) != RESET)
{
__HAL_GPIO_EXTI_CLEAR_IT(GPIO_TO_CHECK_2_PIN);
counter2++;
__HAL_GPIO_EXTI_CLEAR_IT(GPIO_TO_CHECK_2_PIN);
}
if(__HAL_GPIO_EXTI_GET_IT(GPIO_TO_CHECK_1_PIN) != RESET)
{
__HAL_GPIO_EXTI_CLEAR_IT(GPIO_TO_CHECK_1_PIN);
counter1++;
__HAL_GPIO_EXTI_CLEAR_IT(GPIO_TO_CHECK_1_PIN);
}
}
With the debugger, I check with a breakpoint if counter1++ and counter2++ are executed.
The problem is
: In function of the order of init of gpio, just one or the both interrupt work. If I initialize PB4 then PB5 : IT(PB4): NOK, IT(PB5):OK if I initialize PB5 then PB4 : IT(PB4): OK and IT(PB5): OKThe solution:
In the file stm32l0xx_gpio.c, when the SYSCFG->EXTICR register is configured, the mask to clear the interrupt line is false. All the register is cleared, instead of just the line. The code fixed is (line 258)://Original
// temp = SYSCFG->EXTICR[position >> 2];
// temp &= ~((uint32_t)0x0F) << (4 * (position & 0x03));
// temp |= ((uint32_t)(GET_GPIO_SOURCE(GPIOx)) << (4 * (position & 0x03)));
// SYSCFG->EXTICR[position >> 2] = temp;
//bug Fixed
temp = SYSCFG->EXTICR[position >> 2];
temp &= ~(((uint32_t)0x0F) << (4 * (position & 0x03)));
temp |= ((uint32_t)(GET_GPIO_SOURCE(GPIOx)) << (4 * (position & 0x03)));
SYSCFG->EXTICR[position >> 2] = temp; Just a parenthesis is add for the not (~) operator.
@ST microelectronics: Thanks to you to tell me if it's a bug or not. If it's a bug, could you send me a
bug report number to know when this bug will be fixed in the new HAL library. And if you are already a new HAL version ( I work with the version 1.1.0), please send me the latest version.
#bug-hal-gpio-interrupt-stm32l0
2015-03-30 2:18 AM
@ST-Microelectronics : Hi engineers of ST-Microelectronics.
Did you check the bug of my last post? Did you check the test unit of the library?I would like to know if (if it's a real bug) this bug is now known from ST, and it will be fix in the next release of HAL of L0.Thanks you.2015-04-01 11:12 AM
wow, we would have been so hit on that too, thanks for tracking this down!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.