2022-06-24 6:38 AM
Hi,
I'm using a STM32G474VET6 with 2x256K flash size.
My custom bootloader is located in Bank1, won't branch to application program.
The PC counter value won't change when debugging to Jump_To_Application()
FYI, when application code is:
Optimized HIGH:
Startup is located in 0x08039D6C (in bank1).
Optimized NONE:
Startup is located in 0x0804D368 (in bank2).
In both senario the bootloader won't jump to the application.
DBANK=1 and BFB2=0
thanks
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.