2016-01-15 7:18 AM
Hi,
I would like to udpdate the microcontroller STM32F42xxx SW without having access to Boot pins ( hardwired to boot0 = 0 boot 1 = 0) and by using USART port. code is stored in internal flash memory containing SW code ( code run fom flash) through the USART bus by using existing bootloader. I would like this update be protected by password. first operation : during 5 first seconds after start, CPU waits for password through UART. if not received it jump to operational application, otherwise it jumps to bootloader adress in System memory. second operation : terminal sends commands to change flash content to bootloader firmware third operation : exit with go command or HW reset. my question's : -Do you see any difficulties to develop this ? - in case of wrong flash write , power off during flash donwloading,... there is a risk that SW code is corrupted and thus never be able to access flash memory without opening box . Am I right ? or Is a protection mechanism exists that detect invalid I-code ( as soon as one is met) and jump to bootloader ? maybe other alternative to my problem ? Thanks for the Help. Laurent.2016-01-15 7:50 AM
No the processor will just crash if your firmware is broken. It will try to vector off into the Hard Fault Handler.
Suggest you have a small bootloader, that you don't erase/replace, and that it checksums or integrity checks the application image before jumping to it.There aren't that many strong drivers for using the ROM based loader via the serial port, code your own.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.