2025-06-24 7:58 AM
Hello,
we are using a STM32F429.
The bootloader is located in the first 64kB. The firmware in the remaining sectors.
It erases the remaining sectors of the flash and writes the new firmware.
Now, 3.6.5 Read-while-write (RWW) of the reference manual states that "This feature allows to perform a read operation from one bank while an erase or program operation is performed to the other bank."
Does this mean that reads from the same bank as a sector is erased is not allowed?
If so, how should the bootloader update the firmware in Bank 0, where the bootloader sits itself?
Many thanks in advance for your answer!
Solved! Go to Solution.
2025-06-24 8:21 AM
If you read and write from within the same bank, the read operation will block until the erase/write operation is complete. There are no issues doing this.
If in separate banks, they can operate in parallel.
2025-06-24 8:21 AM
If you read and write from within the same bank, the read operation will block until the erase/write operation is complete. There are no issues doing this.
If in separate banks, they can operate in parallel.
2025-06-24 10:22 PM
I understand. Thank you very much!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.