2018-03-21 12:59 PM
I've downloaded the pre-bulit linux image provided by emcraft to STM32F746G discovery board using u-boot. The QSPI entry address is 0x90000000. After downloading the image I wasn't able to boot linux using the bootm command. The syntax is simple: bootm 90000000. I got the following error:
Wrong image format for bootm command
Error: Can't get kernel image
Any help?
p.s.: I am able to download and boot the image from sdram using the same commands
#uclinux #u-boot #emcraft #stm32f746 #qspi2018-03-21 1:14 PM
EmCraft have their own website and support structures, don't expect to see a lot of support for it here.
Dump the data at 0x90000000
Is the data there visible?
Is the image data in the correct format for u-Boot to use?
Is it built for the right memory location?
Can you script u-Boot to copy the image to SDRAM and call it?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.