2024-02-09 1:09 AM
We don't understand the bit SCUEN of STM32H7.
The description is not very clear:
Could you explain what SCUEN means and if the software is supposed to write or read this bit and why ?
2024-02-09 8:46 PM
Where have you seen this? I tried to find in my STM32H7 manuals but I do not see anything for SCUEN.
Where is coming from? (provide doc name, link and page as info, thank you).
2024-02-11 11:02 PM
It's in the technical reference manual, nothing exotic...
Chapter 6 "PWR"
2024-02-12 12:05 AM
No SCUEN bit in RM0468 for STM32H723/733, STM32H725/735 and STM32H730
2024-02-12 12:23 AM
We are looking at RM0433 review 8
§6.4.1
The 21st figure describes the hardware start-up procedure but its unclear wether software or hardware is responsible of its use
2024-02-12 3:44 AM
Okay, RM0433.
You should always say which STM32 / H7 exactly you are using, even in the "basic" registers there seem to be some differences between the H7 types.
I would check how the HAL libraries are using this bit, if they are using it all.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.