2023-03-26 8:45 AM
Dear ST hello,
I am working on a driver on STM32F429, and I have to declare 104 uint8_t buffers.
In some cases I am facing an issue with memory, The buffer is overwritten by another application the buffer values change when I iterate through it the buffer is shifted!
When a loop on the first elements to read and write my buffer it looks very good but when I try to loop on the whole buffer I have a strange behavior.
Some reserved elements should not be changed because I don't change them but I could see them in the watch expression changing.
Do you have any idea to help me debug my problem, please?
Thank you in advance,
2023-03-26 9:52 PM
Share some source code and the linker script.
Then tell us please:
2023-03-26 11:19 PM
Are you using DMA?
What else is writing to the buffer?
Can you take a mutex or semaphore to stop other tasks touching the array?
Do you have an asymmetrical input / output flow rates for the data?
Why is the processing slower than the acquisition?
Can you catch up via dropping occasional packets?
2023-03-27 1:00 AM
Yes, I could share the project,
2023-03-27 1:04 AM
Non, I am not using DMA, the buffer is updated each 10 ms using the spi bus,
I am nothing using RTOS.
I shared the code, the buffer name is GyroAccDriver
2023-03-27 2:14 AM
> the buffer name is GyroscopeDriver
which is declared and used in which files?
2023-03-27 2:27 AM
GyroAccDriver is declared in the stm32f429i_discovery_Gyro_Acc
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.