2017-03-26 10:46 PM
Hello everyone,
I am trying to reverse the motor direction using PWM from the STM32F1 Series controller and using the L293D Motor driver. I have referred to the bi-directional motor control circuit given in l293d datasheet and done connections accordingly. The following is a snippet of the code which I have used to try the direction control.
Please feel free to point out my mistake.
Thanks.
HAL_TIM_PWM_Start(&htim2,TIM_CHANNEL_2);
HAL_TIM_PWM_Start(&htim2,TIM_CHANNEL_3);
__HAL_TIM_SetCompare(&htim2,TIM_CHANNEL_2,1000);
__HAL_TIM_SetCompare(&htim2,TIM_CHANNEL_3,0);
HAL_Delay(10000);
__HAL_TIM_SetCompare(&htim2,TIM_CHANNEL_2,0);
__HAL_TIM_SetCompare(&htim2,TIM_CHANNEL_3,1000);
HAL_Delay(10000);
#stm32 #nucleo #pwm #motor #controlWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.