STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32U5Ax USB issue

I have a problem with USB initialization on those specific MCUs. Initialization function generated automatically by CubeMX hangs on USB_CoreReset function. Specifically on USB_OTG_GRSTCTL_CSRST bit which doesn't want to set after the reset. The Cube ...

mpico by Associate II
  • 3965 Views
  • 5 replies
  • 0 kudos

SysTick_Handler(void) not getting called with STM32L431CBT6

Hi Everyone, I am working with STM32L431CBT6 and STM IDE cube 1.14. I am currently facing the problem that the HAL_delay function is not working. on investigating further I found that SysTick_Handler(void) is never getting called and thus "uwTick" is...

DKhan1_0-1701460683771.png DKhan1_1-1701460976966.png
DKhan.1 by Associate II
  • 5280 Views
  • 5 replies
  • 0 kudos

STM32 with 64-bit Timer

Can anyone suggest me some STM32 or any other Microcontroller with 64-bit of Timer and Highest Clock Frequency?

Md_Aslam by Associate II
  • 8987 Views
  • 10 replies
  • 1 kudos

STM32 HAL - Encoder Interrupt

hi friends,In STM32F412 microcontroller with HAL LibraryI put timer 2 in encoder mode and everything works fineI want, for example, if the counter reaches 1500, an interruption will occur, but I don't want the counter value to be reset after this int...

Why my crc is not configurable ?

I tried to use the hardware crc for my device stm32f103  . But the STM32CubeMX ( version : 6.10 ) doesnot provide any parameters configuration for this IP. The generated  crc.c is as follows :/* CRC init function */void MX_CRC_Init(void){/* USER CODE...

hanguofu by Associate
  • 1701 Views
  • 2 replies
  • 1 kudos

Resolved! Reading ADC issues multichannel

Hi everyone,   I am trying to use multichannel ADC. I have a panel and an ntc for which I have to read the voltage vlaues. I have disabled the continuous conversion.   sConfig.Channel = ADC_CHANNEL_0; // Select channel for NTCsConfig.Rank = 1;sConfig...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.