STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32U5A5 -- I2C Timeout waiting for TXIS flag --

Hello all,I have been trying to get I2C communication working on my NUCLEO-U5A5ZJ-Q board based on STM32U5A5ZJJT6U. First I have used STM32-CUBE-IDE and CUBE-MX to generate code but I was getting error when I try to transmit so I write a custom code ...

ahsank by Associate II
  • 9644 Views
  • 11 replies
  • 0 kudos

STM32 celebrates 10 years of innovation

Posted on July 03, 2017 at 17:16     STM32 celebrates 10 years of innovation   From STM32F1, the world first 32-bit ARM� Cortex�-M MCU announced on June 11th to STM32H7, the world most efficient MCU released in 2017, the STM32 ARM� Cortex�-M microco...

0690X00000603vYQAQ.jpg 0690X00000603vYQAQ.jpg 0690X00000607OTQAY.png 0690X00000607HEQAY.png

STM32F405 UART communication between PC

I am sending a command to the STM32F405 through the UART (COM) port for receiving data from the STM32F405. Once the command send from PC it will continously send data from STM32F405. What if the PC drops the connection and goes to sleep. And my STM32...

cjaya.2 by Associate II
  • 2364 Views
  • 3 replies
  • 1 kudos

Unable to send data over USART1 TX line (PC4) on NUCLEO-G0B1RE

Hi,     Configured PC4 and PC5 for transmitting and receiving over USART1.    Enabled the interrupt, DMA is disabled.     Tried with different baud rates, same results.     The data seen on serial console application cutecom does not match data I am ...

mohitmg by Associate II
  • 2823 Views
  • 5 replies
  • 1 kudos

Resolved! About libraries and SDKs

We are developing using the following development environment. Are there any libraries or SDKs that we can use?Also, Is HAL or LL a library? [IDE] STM32CubeIDE 1.14.0[MCU] STM32F412VGT6

The STM32H562RG USB interrupt does not work.

The STM32H562RG USB interrupt does not work.Also, using the library on the Nucleo-H503RB results in a memory error. We verified the other chips work fine, but the H562RG has a problem with the USB interrupt not working.

sunmk97 by Associate
  • 1588 Views
  • 2 replies
  • 0 kudos

STM32 USB C to UART communication

Hello, I am making a development board where I want to use STM32 and USB C connector for power supply to the STM and also for UART communication with the PC. What are the best solutions for this? I looked into using FTDI chip but they are quite expen...

PPopo.1 by Senior
  • 2219 Views
  • 2 replies
  • 0 kudos

Resolved! STM32U5A Wake-UP from stop mode 3

Hello all, I am using the STM32U5A5QJ in a project and I had a question about some of the wake-up modes. I would like the microcontroller to be in stop mode 3 most of the time until it receives an interrupt from a sensor to return to normal mode. The...

Resolved! NUCLEO-F429 ADC DMA

Hi,I am currently using NUCLEO-F429 for prototyping a medical product.I am facing an issue while configuring ADC DMA as shown in attached image.the address of DMABuff going in DMA register is different to the actual adress, hence i am not able to get...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.