STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Problems with SPI on nucleo H7A3ZIQ

Hey guys. I'm trying to use the SPI1 interface on the aforementioned nuncleo board, but no luck whatsoever.I want to transmit 2 3Byte commands to a dac device. The first one is 48,0,0 and the second one is 55,255,255. My code is:   uint8_t msg_Tec[3]...

427871791_1662620054268756_5368746019243408541_n.jpg 428140409_793728049247140_142200024438007881_n.jpg 427800643_1547669725992226_120932931604016297_n.jpg 427861298_295168103284722_2694724649385907734_n.jpg

Resolved! condition check below low level

Hi,I have question, I wanted to check whether a condition has reached below threshold level. How many check do I need to do whether it has reached the level below. Does it need to be three check or do a 20 check and average out to see if it below tha...

cjaya.2 by Associate II
  • 4086 Views
  • 10 replies
  • 3 kudos

Resolved! Issue with USART RXFIFO threshold configuration

Hello,I am developing an application on STM32H563 MCU and NUCLEO board.I have the following problem when trying to configure USART2 RXFIFO threshold.In particular, on a transmission completed event, inside the ISR, I need to configure the RXFIFO thre...

CTabo.1 by Senior
  • 2195 Views
  • 2 replies
  • 0 kudos

Resolved! STM32H745 SPI Cores communicating

Hi!I'm using STM32H745 dual core. The reason behind it is as I have to do very fast measurement on one core (M7) and the rest of the slower things on the M4. The M4 is mostly used for communicating with the external world. I have setup SPI3 and SPI4....

__silardg by Associate III
  • 7309 Views
  • 13 replies
  • 0 kudos

ADC multimode DMA init error

I am using ADC regular simultaneous mode with stm32f427It works nice with the pulse signal is comming after dma start(HAL_ADCEx_MultiModeStart_DMA)but if the signal is comming before calling ADC dma start code it going to infinityhow to solve this?i ...

SKim1761_0-1707793855535.png
SKim.1761 by Associate III
  • 1066 Views
  • 0 replies
  • 0 kudos

STM32H7 TIM12 TRGO DAC DMA syncronization

Hello,I am trying to generate a pulse-triggered waveform continuously by using DAC and DMA in STM32H735RGV6. To do this, I have opened DAC OUT1 with the following configuration.After that, I set up the TIM12 with the following configuration and expec...

ErsinKuscu_0-1707732708749.png

Resolved! Stm32f410RBT6

Hello, we are a manufacturer company that uses STM products. We developed a device using stm32f410 and stm32f446 products 2 years ago. We have a few processors from this old series, stm32f410 and stm32f446, and they work without any problems. However...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.