STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Cannot access memory

Hi, I am having problem with string copy strncpy(). I am getting error message "Cannot access memory at address 0x31203a6e" static char *DataBuffer[30] = {0}; for(char *str =strtok((char*)recdata, "\n\n"); str; str = strtok(NULL, "\n\n")) { strncp...

cjaya.2 by Associate II
  • 6200 Views
  • 10 replies
  • 0 kudos

STM32L476

Dear Sir,I use NUCLEO-L476 , Once I connect it to usba new window pop up like with the Caption NODE_L476RG .Erasing the CPU still the window pop up.What should I do to make this board to act as plain PCB  

Resolved! stm32f407 Disc and external stlink problem

Hi everyone I'm trying to use external debugger with my stm32 disc1 board. The problem is if i only connect the stlink and my board i can't debug it, but if I power the board with another usb port i can access it.So my question is why do i have to po...

Ahmetp by Associate II
  • 3529 Views
  • 5 replies
  • 1 kudos

STM32F437 External Memory Interface

Posted on April 13, 2015 at 14:00In one of our embedded systems we use a MR256A08B MRAM in conjunction with a STM32F437 microcontroller. Sometimes (increasing with temperature) we are observing the problem that we cannot write to discrete bits of th...

Resolved! Error: Interlacing the process

I am using STM32H7 and using the M4 core to output GPIO to control peripherals.I share data between the two cores using the share memory protocol.On the M4 core, I have turned off all interrupts and only control GPIO, but when measured, there is stil...

H723 Cubemax:SPI cannot recieve data

  I has been devloping an ECG program with ADS1292R and STM32H723VGT6.I has been struggling with a problem. The ADS1292R uses SPI and it's register can be read if I use STM32C8T6 which configuerd by libray finction.But when I configuer program with H...

begall_0-1708768046408.png begall_1-1708768087740.png
begall by Associate II
  • 3978 Views
  • 7 replies
  • 2 kudos

Resolved! STM32F103C8T6 does not seem to have RTC wakeup feature?

Hi, I am trying to use STM32F103C8T6 standby mode and wake it up with wake up feature of RTC, but in CubeMX I don't see that this MCU would have wake up feature under RTC settings. How do I wake up this MCU from standby with RTC and wake up pin?  

JBond1_0-1708777906165.png
JBond.1 by Senior II
  • 1597 Views
  • 1 replies
  • 0 kudos

Keeping data on multiple STM32s in Sync

Hello,I need guidance on how to best implement a packet protocol to keep the data on multiple STM32F373 in sync with each other.  If possible, I would like to reach a 'refresh rate' of 30ms.  Packet payloads for data refreshed could be up to 50 bytes...

LMorr.3 by Senior II
  • 3629 Views
  • 6 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.