STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Fault handler, stack frame

Hi.I am trying to test out a fault handler for our STM32G (right now, the fault handler just tries to determine the location of the code that caused the fault).If I force a fault (divide by zero) in "normal" non-interrupt handler code, I can easily r...

Resolved! RM0394 SRAM2 connectivity in bus matrix

In the lower-end STM32L4, covered by RM0394, SRAM is partitioned into two parts, SRAM1 and SRAM2.SRAM2 (besides being "special" in that it has ECC and automatic erase facities), is mapped at both 0x1000'0000 and at the end of SRAM1 in the 0x200x'xxxx...

waclawekjan_0-1764945335823.png

STM32G0: Encoder mode + Output Compare

I am using STM32G071RBT6. I am trying to implement encoder mode + output compare mode using same timer. Right now initially I get OC interrupt even when Tim_CCR3IF flag is 0 and once it get set it remains as it is. - Should I combine encoder and OC m...

Resolved! USB Descriptor Table and PMA Layout on STM32F103

Hi, I’m trying to better understand how the USB PMA and BTABLE work on the STM32F103. After reading the reference manual, I’m still unsure how the descriptor table size relates to the number of endpoints.I have two possible interpretations of how the...

STM32-USB-PMA-update.png
rohamid by Associate II
  • 770 Views
  • 2 replies
  • 0 kudos

Resolved! STM32 l476rg CAN not working

I am using STM32 Nucleo-l476rg. I am trying to use the CAN peripheral and have tried every resource I came across. I am unable to send or receive messages:I have no filter, everything is wired correctly, what could be the issue? I even made it so tha...

at3 by Associate III
  • 5126 Views
  • 10 replies
  • 1 kudos

STM32H533CET6 ADC Reading

I am encountering an issue with ADC readings on a custom board based on the STM32H533CET6.Hardware Setup: I have a simple analog filter connected to the ADC input. I have verified the input signal with a multimeter, and it correctly varies from 0V to...

obraz (9).png obraz (8).png obraz (7).png obraz (6).png
Karol123 by Associate
  • 628 Views
  • 3 replies
  • 0 kudos

STM32H743 as USB Host stops communicating

Hello, I have a problem that I am having a hard time figuring out.My project is using an STM32H743 as a USB host on a custom PCB. Both OTG_HS and OTG_FS ports are connected to different devices. OTG_HS is using the internal PHY and operating at full-...

Resolved! Ruling out fake STM32G474s

Hi,I'm facing some issues with some STM32G474RET6s, and want to rule out counterfeit chips, even if that seems unlikely.After googling for some solutions, I confirmed the AP IDR register and the DBGMCU_IDCODE both hold a revision ID of 3, which I exp...

stm32.jpg abond_2-1755301541101.png
abond by Associate
  • 1590 Views
  • 8 replies
  • 3 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.