STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Different binary data when running directly

Hello,I have a strange problem that I already lost a lot of hair over. I am using cubeIDE with an stlink v2 (STM32G441 with a blank C/C++ project and CMSIS). All run very well until today. So I am sure the code itself is ok.If I compile the project b...

STM32F0 HDMI

I'm working with stm32f0 hdmi cec function to make Arc audio with tvI can able to communicate with tv but arc not initiate with feature abort commandAnyone have used it before help me with source example

DHANA by Associate
  • 868 Views
  • 0 replies
  • 0 kudos

Nucleo board 64 F070 Crystal output Problem

Hi 'I am using STM32 Nulceo Board Nucleo-F070RB .I tried some projects but the output of the project is not as expected ,shows some wrong calculation out .So I checked everything ,And found out the Crystal frequancy is not correct .I checked the Mast...

STM32F103C8T6 drive camera ov2640

I have used software control GPIO simulate parallel interface to successfully receive data, but how to faster, I used timer to trigger DMA, but the effect is very bad.stm32f1_ov2640_tim_dma_uart About: 1-1.5 FPS

Shiina_0-1714231947043.png
Shiina by Associate III
  • 10216 Views
  • 2 replies
  • 1 kudos

DS18b20 temperature sensor does not work with STM32L073RZ microcontroller, Can anyone help me to find the error

I am working with DS18b20 temperature sensor in STM32L073RZ board. DS18b20 works using one wire communication. I used one GPIO pin for communicate with DS18b20. i couldn't get the sensor reading. i have attached my code below. Thanks in advance.sta...

Resolved! VSCode Debugger Breakpoints jump

HiI am having problems setting breakpoints when using the debugger in VS Code. I can step through manually but cannot seem to set breakpoints. Before starting to debug I can add a breakpoint at 50But when I run the code the breakpoint changes to a di...

bibble235_1-1714222278230.png bibble235_2-1714222427049.png
bibble235 by Associate III
  • 4066 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.