PLC Likes ON-PULS
I would like to generate a pulse by timer.Idle state: GPIO-PIN HIGHafter internal trigger: GPIO-PIN LOWafter 1us back to GPIO-PIN HIGHi have try by PWM, OC and one pulse enabled mode.but my pulse is starting after 1 us.
Ask questions, find answers, and share insights on STM32 products and their technical features.
I would like to generate a pulse by timer.Idle state: GPIO-PIN HIGHafter internal trigger: GPIO-PIN LOWafter 1us back to GPIO-PIN HIGHi have try by PWM, OC and one pulse enabled mode.but my pulse is starting after 1 us.
Hi,I have been working on, interfacing PSRAM(APS6404L) with NUCLEO-H563ZI board.i'm able to perform read and write operations using QSPI and able to create the memory mapped mode. I have modified the Linker script,i'm able to declare variables on ext...
I've done a long search on the Internet but only found the migrated STM32F103 to the STM32F4 series, not vice-versa. So I'm asking anyone who can help me. To be specific I am going to try this project from GitHub but in my case, I'm going to use STM3...
Hi, We want to use now the STM32H5 for future projects. In the past, we used STM32F4 with enabled SWO for debugging. Is there any example available to get this feature working for STM32H503? Would be great to do it on register level to be independent...
We are using STM32F373VCT6 Microcontroller for our application and we want to use an External Flash Memory of 1MB with this controller. Can you suggest some NAND/NOR Flash memory of 1MB, that supports SPI/QSPI and is compatible with this controller a...
Heyho FLASH experts!within the last few weeks I was able to get an ethernet bootloader running on a H735 discovery kit.Internal flash is partitioned into area starting with the bootloader (256kB, including ETH), then comes the application (rest: 768k...
I have a custom PCB based on STM32F767 which has been working for about 2-3 weeks, through about 100 re-programming cycles (doing debugging). Now, after last attempt to flash, the NRST pin is "stuck" to VSS. I lifted the pin of the trace, e.g. NRST p...
Where can I find the DSP library for the STMF7 processors? In the CMSIS DSP Software Library documentation I read that I can use the arm_cortexM7lfsp_math.lib (Little endian and Single Precision Floating Point Unit on Cortex-M7). On the website of ST...
Hi i am planning to use internal comparator.The propagation delay for comparators are 31nS which is at 25 deg CCan you please let me know what is the all drifts and all propagation at 125 Deg C? Thanks
I've got an black pill with STM32F411CEU6 on it, I plan to simply use it for a single purpose: reading ADC at near full capacity and transfer values to PC via USB. After investigating around F411 product page on st.com, I've found that:ADCin product ...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.