STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32U575 debug access

I've built a new prototype using the STM32U575C, and provisioned two program/debug connectors, a fine pitch Samtec header and 0,1" pitch six pin header, I've used both before on STM32F4.I've tried accessing the processor using both headers, an STLINK...

After sending I3C broadcast, loops in Error_Handler

The project code for my Nucleo-H563ZI sent an I3C Broadcast sequence for dynamic addressing. I can see the Broad cast sequence on the analyzer. There currently is NO I3C Target on to answer, yet the analyzer does show a NACK after RnW(1). I believe t...

JRM_02 by Associate II
  • 1135 Views
  • 1 replies
  • 0 kudos

SPI for LCD failed to transmit data on STM32F103VET6

I'm trying to initialize an LCD module (ST7796U controller) on a STM32F103VET6 development board using SPI1, yet the souce code I got from the seller is using software-simulated SPI instead of hardware SPI (with SPI1_NSS enabled as output):   #define...

OW1TY2 by Associate II
  • 3456 Views
  • 2 replies
  • 1 kudos

Resolved! STM32H7 USB Low Speed Enumeration fail issue

Hello,Greetings to all community members, This post is regarding USB enumeration in STM32H7 series. I am currently using MCU STM32H747XIH6 for one my project in which I am configuring this MCU in USB Host by using USB_OTG feature available in it. I a...

Resolved! How the H750 kernel is powered using an external power supply

When using the STM32H750VBT6, I supplied around 1.37-1.4 supply voltage to the external pins VCAP1 and VCAP2,the project was configured as an external power supply using cubemx software.HAL_PWREx_ConfigSupply(PWR_EXTERNAL_SOURCE_SUPPLY); is used in t...

allgoodhi_0-1715329182041.png allgoodhi_0-1715328294289.png
allgoodhi by Associate II
  • 2460 Views
  • 3 replies
  • 1 kudos

Resolved! Detecting JTAG Access on the Board

Hi, I am using the B-U585I-IOT20A Board and I want the board to notify me in some way if someone is attempting to access and modify its content via JTAG. Is there a way to do this?

STM32F765VGT6 with 216MHz CPU clock frequency

I designed a circuit board with the STM32f765vgt6 chip following ST's hardware recommendations (two 2.2uF ceramic capacitors with low ESR connected to Vcap1, Vcap2).I'm having the following issues: When I initialize the CPU clock frequency to 216MHz,...

Resolved! STM32L475 and URC's management via UART

Hello,I'm managing a Wifi modem using one of the USARTs of the STM32L475.Modem is working fine when sending and receiving AT commands and data, but I'm not able to receive URC's.I only receive URC's when they come 'together' (very close) to the answe...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.