STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! LPUART no output

Hello,I am programming an STM32WB55CGU6 on custom PCB. I'm using the LPUART1 peripheral according to the datasheet and reference manual, but at the transmitter pin (PA2) I'm not seeing any traffic. It's just stable at about 3.3V. There is a led at PC...

JS8 by Senior
  • 1922 Views
  • 2 replies
  • 0 kudos

How to: STM32F103C8T6 in a PCB design?

I'm a beginner so bear with me:I am making a calculator with a STM32 Blue Pill and would like to create a PCB so that the calculator can be decently compact. I am unclear on some things though. Is it normal to place the entire Blue Pill in a PCB desi...

Jordan1 by Associate
  • 2690 Views
  • 1 replies
  • 1 kudos

Resolved! HAL Function CRC Accumulate != Re-Init and Calculate

I have gotten the following code to correctly validate CRC's, so I know I have configured the CRC correctly: uint32_t calcCRC = 0; hcrc.Instance->INIT = 0xFFFFFFFF; calcCRC = HAL_CRC_Calculate(&hcrc, (uint32_t*) pointer, length); calcCRC = HAL_CRC_Ac...

astral256 by Associate II
  • 4073 Views
  • 3 replies
  • 3 kudos

Ethernet Communication

Posted on February 20, 2013 at 06:33I am using STM32F107RB for Ethernet Communication. If i am using only one STM32F107RB module there is no problem but when i connect two modules to two different systems via modscan32, one of the module responds pr...

aru by Associate II
  • 6326 Views
  • 15 replies
  • 0 kudos

STM32H7R3 and DMA speed

I want to use fastest STM32H7R3 at 600MHz clock.I need to use 60Mbytes/s short term DMA transfer from GPIO data 8-bit bus to RAM (about 1kbytes stream), driven from external clock, with up/down external clock slope (30MHz external clock with upslope ...

wadi by Associate II
  • 1542 Views
  • 1 replies
  • 1 kudos

Enabling ADC interupt while HAL_ADC_Start_DMA using

Hai allWhen I use HAL_ADC_Start_DMA(&hadc, ADC_RES, 160); this function .How to enable ADC interupt bit .I want to Trigger void HAL_ADC_ConvCpltCallback(ADC_HandleTypeDef* hadc){ HAL_GPIO_TogglePin(GPIOC, GPIO_PIN_6);}this funtion How to enable it wh...

Resolved! STM32F103VET6 boot problem

Hi,I want to use PB3 an PB4 pins as SPI1. When i use st-link and debug my code, it works. but when i plug-off st-link it seems that mcu can not boot. I use the codes below for jtag disable , but it does not work. Any advise for my problem? GPIO_InitT...

er3481 by Senior
  • 2289 Views
  • 4 replies
  • 2 kudos

Low power using ST-Link to Power Nucleo-144

I trying to program a nucleo-144 L496GZ-P board which has been split from the st-link. I've connected the SWD pins as instructed in the user manual (SWD1 -> 3v3, SWD2 -> SWCLK (CN11 P15), SWD3 -> ground, SWD4 -> SWDIO (CN11 P13), SWD5 -> NRST (CN11 P...

froggiee by Associate
  • 845 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.