STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

2(two) USB-2.0_FS Working

hi , i need   manage one usb  pendrive and usb keyboard in USB_fs mode .it's possible to use 2 USB_FS mode simultaneously like One is HOST+mass storage  and Another One is for HOST+HID can anyone please suggest . Cube ide able make the code generatio...

MMARI.1 by Senior II
  • 4658 Views
  • 8 replies
  • 0 kudos

CoIDE - and CooCox - dead?

Posted on March 21, 2018 at 12:24CoIDE is still listed as 'Active' by ST: http://www.st.com/content/st_com/en/products/development-tools/software-development-tools/stm32-software-development-tools/stm32-ides/coide.html But it seems that CooCox and C...

0690X0000060ABNQA2.png 0690X0000060ABmQAM.png

Resolved! Issue casting an integer type to char type/string

Here is the method defined in the .h file: void ILI9341_DrawText(const char* str, const uint8_t font[], uint16_t X, uint16_t Y, uint16_t color, uint16_t bgcolor); the method defined in the .c file: void ILI9341_DrawText(const char* str, const uint8_...

NUCLEO-STM32U083RC HAL_UART_Receive reads nothing

Hi all,I have recently purchased a U083RC core and I am having problems reading data using USART1 under Single Wire (Half-duplex mode).I am connecting to a sensor that only uses a single wire to send and receive data using a custom protocol running a...

husq by Associate
  • 1443 Views
  • 1 replies
  • 0 kudos

STM32G0C1CEU RTC_REFIN and GPIO Input state

HiI am designing PCB with the MCU above. I do not have any devboard for now with G0 to check what I need.I want to utilyze the REFIN function of the RTC. I also need to check presence of this signal (if there is no 50Hz signal for some time [few 100'...

Resolved! stm32h747 discovery blank

i just received my brand new stm32h747 discovery board, on power-up it does nothing just two LEDs light up, according to the user manual it should be preloaded with a demo.I checked in cube prog and it reports as blank.Is it possible that my device g...

Resolved! STM32G4 dithering + DMAR + 16bit access

There is glitch when accessing timer registers using DMA- Halfword memory to halfword peripheral DMA transfer- DMA target is TIM15->DMAR, configured to write ARR register.- TIM15 dithering enabledUnder these conditions, bits from ARR[3:0] will end up...

ledvinap by Associate II
  • 3593 Views
  • 6 replies
  • 2 kudos

Kit cables

Hello, got Nucleo F439 kit, amazed to see no cables in it.Wanted to check if the cable "USB Micro-B connector (CN1)" is same for "USB Micro-AB connector (CN13)" connected in reverse?Cause Im not able to identify cable "USB Micro-AB" to buy.

GauravK by Senior
  • 1513 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.