STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! external RAM for stm32h753zi

Hi, my program required a large amount of RAM memory, how can i know which external memory i can choose? and which peripheral is dedicated for this? 

Ditzhak by Associate III
  • 2816 Views
  • 4 replies
  • 0 kudos

ADC polling of multiple channels

Hello,After setting up a 4 channel read with DMA, I ran into the problem, that the value of the internal temperature sensor seemed to not change at all. The values of the read out potentiometer however were plausible.So I wanted to check all used cha...

Resolved! HAL_I2C_Mem_Write_DMA issue

Hi There,I have searched a lot about the  HAL_I2C_Mem_Write_DMA problem and seems like i have not found anywhere else this issue has been solved.Can anyone contribute if someone has solved it. Thanks

Resolved! STM32h7b0 - System memory bootloader AN2606

Hi, I'm having issues on our custom board jumping to the system memory bootrom.Likely i have a software issue but would like to clarify the system memory address for the bootloader. This is usually listed in AN2606 but there is no explicit mention of...

Resolved! How do I change the Baud rate of a UART/USART whilst running?

I've followed some answers from a post here:https://stackoverflow.com/questions/57283327/how-to-change-the-uart-baud-rate-after-running-on-stm32-boardBut still can't seem to get the baud rate to change. Has anyone had any luck trying to dynamically c...

C.East2 by Associate III
  • 15658 Views
  • 11 replies
  • 2 kudos

Regarding Volatge Control in STM32L562CET6

Hi all,          I have working on USBPD Sink project in that ,I have been struck in the part of reading the voltage from the STM32L562CET6(Customized Board)before this process I have done the same project in STM32L562E-DK , What I need to do actuall...

nishadh by Associate
  • 851 Views
  • 0 replies
  • 0 kudos

Measure STM32F373 core temperature

Hi,I was measuring the STM32F373 core temperature.It seems that the core is 56°C while the environment is 23°C, no housing.Is the 56°C a reasonable temperature? It looks quite high to me.I used the settings below:

ADC_Temperature.png
BPutt.1 by Associate II
  • 1328 Views
  • 1 replies
  • 1 kudos

Resolved! Mixing HAL and Direct Register Manipulation

Hello. I am writing a code to read ADC data from an AC voltage sensor. I used HAL to initialize ADC 1 and USART2 for checking the values in Putty. However, I would like to use direct register manipulation to send data to USART6 so that it can transmi...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.