STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

UART in STM32-L432KC

This is regarding the UART1 and UART2. 1. I am trying to learn how UART works by communicating between STM32 and ESP32. I am able to send data from STM32 to ESP32 and it works. However, when I do the same from ESP32 to STM32, for some reason I cannot...

Abijith by Associate II
  • 6087 Views
  • 9 replies
  • 1 kudos

SMBus blocked and how to recover it

Hi ST tesam,When I use the HAL of STM32C031, I have some trouble about SMBus.Q1:When I use the SMBus of STM32C031 series. If I do not got the feedback from the slave, sometimes the SDA will pull down(similar to the yellow line show as below) and syst...

LsnLeeJW_0-1719216894031.png
LsnLeeJW by Associate II
  • 1183 Views
  • 0 replies
  • 0 kudos

Resolved! How to configure STM32F407VG using Ethernet in ENC28J60

Hi Team, where we are trying interface ENC28J60 in STM32F407VG Microcontroller to use Ethernet, Is there any procedure to create a project in cube ide are any link related to this board how to interface ENC28J60 to STM controller. Best Regards,Gagan ...

ggowd.1 by Associate III
  • 5449 Views
  • 7 replies
  • 2 kudos

ARM exception STM32f203 based Micro

Working on a product-based STM32F203, getting multiple ARM exceptions of all kinds, Bus Fault, Usage Fault, Hard fault, and Mem fault. The issue is I have a year-old debug Log for debugging purposes. I can't recreate any ARM exception to check the st...

Dev3835 by Associate
  • 1397 Views
  • 1 replies
  • 1 kudos

2 Nucleo as slave to Modbus master

I want to connect 2 Nucleo F103RB as slave (2 Nucleo slaves) to one master (PC for now) over Modbus (RS485). how can I do that? Please note I am new to STM32, so I have limited knowledge.P.S. I have connected one master (PC) and one slave (Nucleo) bu...

Resolved! STM32L476RE output characteristic impedance

Hi team,I am currently developing a board with the STM32L476RET6. This project involves UART communication (UART4, PA0 and PA1), and I am concerned about EMI due to the fast rising and falling edges of the TX signal. To address this issue, I am imple...

LucasRosa by Associate III
  • 5724 Views
  • 9 replies
  • 2 kudos

Resolved! Stm32f429zi RCC setup

Hi!I'm using Nucleo-f429zi board and my trying to configure it to read and write data over modbus RTU (RS485)and i'm using keil uvision 5 to program. I have referred some videos and post on how to configure STM32 and its USART port for modbus communi...

jared212 by Associate
  • 1392 Views
  • 1 replies
  • 0 kudos

STM32U5A5 GPIO state change on Stop2 mode enter

I am trying to figure out why the state of GPIO pins are changing after entering Stop2 mode. I've got an ADC chip connected with Reset lines being held high by GPIO pins configured as push-pull with pull-ups enabled. When the device enters Stop2 mode...

ocean_rse by Associate II
  • 1646 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.