STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! While Syntax Error in STM32F105 using KEIL compiler

we have assigned a while condition below the given code, even if the condition is false, or the while condition gets 0, the code also does not execute, it stucked at program counter on while only, if I entered a delay of 1 ms, using Hal_delay after W...

stm32wb5mmghtr ADC value Error

I have been working with the STM32WB5MMG-HTR controller and have configured ADC1_IN4 (PC3) for ADC value readings. However, I consistently receive a stable ADC value of 4096. Could you please confirm whether I am reading the value correctly? I have a...

_Danny_ by Associate III
  • 1328 Views
  • 1 replies
  • 0 kudos

LPBAM Scenario usage multiple analog watchdogs

I've trying for days to get the LPBAM tool to work. The TempSense example project is similar to what i'm trying to do. I'd like to immediately stop2 on power up and continually sample 3 channels. The first condition i'm waiting for is IN1 > 1100, ...

_legacyfs_online_stmicro_images_0693W00000bkVWSQA2.png
sleon.1 by Associate II
  • 3908 Views
  • 6 replies
  • 0 kudos

Resolved! Is it possible to download firmware using UART?

I'm using STM32H733VGT6, STM32F030CCT6 and LTE module. As show as attached picture, it is conneted via UART. I want to recieve data through LTE and connect STM32H733VGT or STM32F030CCT to DFU to download firmware. Is it possible with UART? STM32H733V...

STM_attached.png

Tag connector on STM32H735G-DK.

HiI'm designing a PCB using the STM32H735 based on the eval kit STM32H735G-DK.On STM32H735G-DK there is both STlink connector and a TAG Connecter, but they are not wired the same way.I have the STlink working but was wondering what type of programmer...

Kvang by Associate III
  • 774 Views
  • 0 replies
  • 0 kudos

Resolved! SAI1 DMA Callback Issue

Hello everyone,I'm currently working on a project using the STM32H723VE microcontroller and have encountered a problem with the SAI1 peripheral. Previously, I developed my code on the STM32H723ZG Nucleo and everything worked perfectly, including the ...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.