STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

half a USB problem on STM32F401

Hi I designed a replacement pcb for a keyboard of mine with an STM32F401(RCT6).I used the QMK framework to make a firmware which I can download via DFU perfectly fine (I also uploaded it and checked it against what I downloaded..). The PC detects the...

blap by Associate
  • 1862 Views
  • 1 replies
  • 0 kudos

STM32 to StM32 with SPI

I know there are hundreds of posts about this and I've been through most of them but still can't get things to work.The concept is simple: set up 2 Nucleo F446 boards, one as full duplex slave the other as full duplex slave.Master pseudo code:while 1...

Greybeard by Associate II
  • 6482 Views
  • 6 replies
  • 0 kudos

Resolved! External Loader in SPI mode

Hi I am using Stm32L0 series board to create a custom external loader. I am using cubeIDE (version: 1.16.0)I am using winboard W25Q64 chip. I wrote a driver for this chip and interfaced it to my mcu using standard SPI2. I can read /write data on this...

zain_stm32_0-1725837097637.png

STM32L562CET6

I want to create USB PD Sink Demo on STM32L562CET6, i referred the below demo.LINK Below:STM32L562 EDK USB PD Demo from STM32 is that possible recreate the same demo to the STM32L562CET6 or any changes need to be do because i didn't get any output vo...

STM32F407ZGT6 to LTC1859IG read issues

Hi all,First post here...I'm fairly new to STM32, working on STM32CubeIDE and have running code on a very well designed and laid out PCB with above components being the main actors.. The project was setup with STM32CubeMX V6.4.0 using STM32Cube FW_F4...

lebies by Associate II
  • 1927 Views
  • 3 replies
  • 0 kudos

Appropiate board for real time sound classification

Hello,I was trying to do sound classification with a STEVAL-STWINBX1. As using a NN directly in a microcontroller is impossible due to ram constrains, I decided to do a basic mel spectrogram (no full mfcc, I skip the dct and log stuff in order to spe...

AlbertG by Associate II
  • 2733 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.