STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Minimum Vbat level for TAMPER detection (STM32G491)

Hi, We have an application on STM32G491 where need to detect a button press after the device was switched off for some minutes. To implement this, we connect a standard capacitor (100 µF) to Vbat pin, Activate battery charging to load the capacitor, ...

SD card to USB data Copy using the CH376s IC

Hello,   I am Use the STM32F091 controller Now we are facing issue on data copying from SD card to USB pendrive. error is "No Free Sector available" Ping is ok, File is open all are ok only problem on last phase How to resolve that ? Please suggest m...

YShah.1 by Associate II
  • 2730 Views
  • 4 replies
  • 2 kudos

Resolved! Hide compiler message

Hi all,Is there a way to hide the console-terminated output message?Per the attached imageI need to remove specifically the timestampthanks 

vicvicvar by Associate II
  • 2086 Views
  • 2 replies
  • 0 kudos

To add a CRC32 result to the end of a bin file,

hiTo append a CRC32 calculation result, which is computed by the hardware CRC ,I want make the crc result  at the end of the bin file , for the purpose of verification during program upgrade.please Give a method,It is best to directly generate the bi...

zhaowhong by Associate III
  • 3116 Views
  • 6 replies
  • 1 kudos

Resolved! Timer isn't accurate

I am using an stm32 timer calculator ( https://deepbluembedded.com/stm32-timer-calculator/ ) to get the settings for a 20ms timer and got the following values: https://imgur.com/a/oMHS17r which I set for my TIM16 timer.I am using the following code:v...

DavidL_ by Associate III
  • 1635 Views
  • 2 replies
  • 0 kudos

Resolved! STM32H7S7 XIP Nor Flash + Internal Ram not an option

Previous post here didn't seem to get answered, so I thought I'd ask again.Is there a way to execute code with the XIP framework, but not using the external SDRAM for instruction execution?I'd like to use internal AHB or AXI Ram sections for code exe...

halfordC by Associate II
  • 2301 Views
  • 3 replies
  • 0 kudos

Resolved! STM32G474 use boot0 pb8 pin as I2C1 SCL

Is it possible to use pb8 (boot0) as I2C1 SCL pin, it seems STM32CubeIDE let's me configure it that way. But how can I prevent issues with the boot function after reset? Since I2C is pull-up level, right?

CyberNerd by Associate III
  • 1898 Views
  • 1 replies
  • 1 kudos

Resolved! How to design USB for STM32F105VCT6

Hi All,I want to design USB schematic for STM32F105VCT6. I read Introduction to USB hardware and PCB guidelines using STM32 MCUs(AN4879) and it said that STM32F105/STM32F107 has Pull-up resistor on USB_DP line.Question 1Can I design USB schematic wit...

Capture.PNG
WPong.1 by Associate III
  • 4439 Views
  • 4 replies
  • 2 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.