STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Reset button not working

I am using stm32f103c8t6 microcontroller for uploading the bootloader and application. After uploading the bootloader binary code using UART communication (boot1=0 and boot0=1) to the controller, the reset pin is not working for further functionality...

Resolved! External 24bit DAC interface with nucleo board

I need to generate the millivolts of range between (-10mv to 100mv) with three decimal point accuracy using 24-bit external DAC interfaced with NUCLEO-L496ZG board. Is it possible to generate the range?I need HeadsUp & suggestion to achieve the menti...

akash07 by Associate II
  • 3606 Views
  • 6 replies
  • 3 kudos

Resolved! stm32f103re CRC ?

 hi i used of CRC in stm32CubeMX and for check true worked CRC used of two online CRC calculator site:https://www.sunshine2k.de/coding/javascript/crc/crc_js.html&https://crccalc.com/?crc=123456789&method=&datatype=0&outtype=0 i think stm32cubeIDE int...

kshin.111 by Associate III
  • 3141 Views
  • 6 replies
  • 7 kudos

OSPI Clock Configuration on STM32U5A9J-DK

Hi, I am currently working on configuring the OSPI clock for the STM32U5A9J-DK board, and I have some questions regarding the configuration. From my understanding, based on the Clock Configuration tab in the STM32CubeIDE (.ioc file), the clock going ...

sohm by Associate III
  • 2503 Views
  • 2 replies
  • 1 kudos

DMA latency

I working through issues on an STM32G4 where at times I'm not getting the reaction time from the DMA that I would like. I read AN2548, and it is a very helpful resource. However, I'm seeing slightly worse response times than AN2548 would suggest, and...

tek00077.png tek00076.png
Lee3 by Associate III
  • 2503 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.