STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

I2c problem

Posted on September 06, 2011 at 20:51HiI have a small problem that I hope you can help me with. My problem I that the I2C communication stops after some time.I have 2 IRQ, one I2C and one timer 3 update with highest priority, TIM3 interrupt with 20k...

spa23 by Associate III
  • 2298 Views
  • 5 replies
  • 0 kudos

STM32L15x MPU documentation

Posted on September 07, 2011 at 14:21Hello, In the datasheet I can read, that the STM32L15x has a MPU. But I didn t find anything about it on the RM0038 reference manual. Does anybody know, where the documentation to the MPU can be found ? Is it the...

uwe2 by Associate II
  • 1822 Views
  • 3 replies
  • 0 kudos

STM32F103ze Eval Board

Posted on September 06, 2011 at 10:03I need to use Ext SRAM in my application.In order to understand how to initialize and use it for read/write, I went through the Data sheet as well created a project from the sample code provided for SRAM under fo...

shrinath by Associate II
  • 2181 Views
  • 4 replies
  • 0 kudos

Free toolchain for STM32F2xx series?

Posted on September 06, 2011 at 15:29I just built a board only to discover that the Ride7 + RKit-ARM toolchain does not support the new processors without an expensive support contract.Is there a truly free toolchain that supports the new processors...

szbrozek9 by Associate II
  • 1149 Views
  • 4 replies
  • 0 kudos

Strange ADC and DMA problem

Posted on August 30, 2011 at 10:51The original post was too long to process during our migration. Please click on the attachment to read the original post.

karsten23 by Associate II
  • 1717 Views
  • 7 replies
  • 0 kudos

5V pin no longer supplies 5V; other problems too

Posted on September 02, 2011 at 00:48Yesterday I hooked up my STM32VL Discovery board as the 5V power source for a simple circuit (powering the STM32VL itself from USB). It worked fine. However, today the 5V pin is only supplying about 3V (and the 3...

mastyskal by Associate II
  • 2895 Views
  • 5 replies
  • 0 kudos

STM32F103C8T6 SPI problem

Posted on August 31, 2011 at 15:16Hi, I am trying to establish communication between STM32F103C8T6 and an ASIC using SPI.The STM32 is the master and the ASIC is the slave. The requirement of the ASIC is that it requires the MOSI line to be high duri...

flash word write and byte write

Posted on September 01, 2011 at 22:32Hello,I am using the STM32F series. Right now I am writing to the flash one word at time. I have no problem doing this. I now implemented a function that writes one byte at a time. When I try to do this, I get th...

whitney by Associate II
  • 1943 Views
  • 3 replies
  • 0 kudos

Is any redundancy necessary when using USB HID stack ?

Posted on September 02, 2011 at 14:35Hi all, I am using ST's USB HID stack on an STM32. I communicate with a PC software, and I sometimes got strange behaviours, but I'm not sure if it comes from wrong data during communications. So, I wonder if I n...

Kuikui by Associate III
  • 742 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.