2011-09-06 1:03 AM
I need to use Ext SRAM in my application.In order to understand how to initialize and use it for read/write, I went through the Data sheet as well created a project from the sample code provided for SRAM under folder called FSMC under Keil/arm/example/ST/STM32F10xFWLib/Example/FSMC
However this program does not run though no compilation error. In debug mode on tracing, when it is inside FSMC_SRAM_WriteBuffer any write to Ext SRAM displays no permission to write in the command window (similar if I try read to verify data written, shows no permission to read message).Went through the code it appears to have all initialization required for the control bits and timing register.Can some one let me know what changes to be done in which file? Thanks, shrinath regards2011-09-06 1:52 AM
''any write to Ext SRAM displays no permission to write in the command window (similar if I try read to verify data written, shows no permission to read message)''
This sounds like you have not correctly configured your Keil Project settings to tell the debugger:
http://www.keil.com/support/man/docs/uv4/uv4_cm_map.htm
http://www.keil.com/support/man/docs/gsac/
2011-09-06 6:50 AM
Thanks for suggestion, it appears to have resolved a part of issue, though the write function is not writing data(read from Txbuffer) at address mentioned(Ext SRAM) in the function.
shrinath2011-09-06 7:18 AM
Well, I configured the Target with the following inputs:
Read only memory areas: IROM1 : x08000000 size:0x80000 Read/write memory areas: RAM1: 0x68000000 size 0x10000 IRAM1:0x20000000 size:10000 now it displays no permission to write in the place where the write operation is happening. in the example it needs to write at 0x68008000. thanks, shrinath2011-09-07 6:57 AM
Well, modified the Target option configuration :
removed internal RAM region changed it to Ext SRAM it works now, so now I have two Ext SRAM region.RAM1 and RAM2. ThanxWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.