STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Interrupts priority

Posted on November 13, 2012 at 13:11Hi all Can higher priority interrupt interrupts lower priority in his execution? For example. When I am servicing DMA ISR routine with priority 0x01 and EXTI interruption with priority 0x00 if and only if happens....

DmA for dummies..?

Posted on November 13, 2012 at 18:46Hi. My name is Steve. I have some microcontroller experience with AVR, Stickos and Arduino and have recently bought an STM32F4 discovery kit as I am interested in its DAC , DSP and audio capabiiteies. I have some ...

sts0340 by Associate II
  • 1008 Views
  • 1 replies
  • 0 kudos

STM32 DAC Monotonicity vs DNL

Posted on November 13, 2012 at 11:33I was planning on using an STM32F103RE in a design where the DACs would be part of a control loop, and will need to be used in 12 bit mode.  Unfortunately the DAC specifications in the datasheet show extremely bad...

floating point calcultations within interrupts

Posted on November 04, 2012 at 10:25Hello, I am experiencing some troubles recently with floating point calculation within interrupts. I have a dma interrupt running at 400 Khz in double buffer mode. I have an usart RX interrupt coming at 50 Hz. the...

longchair by Associate III
  • 2949 Views
  • 4 replies
  • 0 kudos

Discovery-F3, Dedicated Forum?

Posted on November 08, 2012 at 15:51I see that there are dedicated forums for some of the STM32 Discovery boards, such as the Discovery-F4. Will there be a dedicated forum for the Discovery-F3? The dedicated forums are a little hard to find because ...

kornak by Associate II
  • 2803 Views
  • 6 replies
  • 0 kudos

Vbat problem on a STM32F4

Posted on June 06, 2012 at 15:59Hi,I'm working on a custom design with in a STM32F4xx. A 420mF capacitor is connected to Vbat. ( with a serial diode and a resistor between Valim and Vbat to charge up the supercapacitor ).The system power off it stil...

stlink v2 under windows8

Posted on November 08, 2012 at 16:52can't install drivers under windows 8, the ''unsigned driver '' error appears. workarounds with reboot to troubleshoot menu does not work because there is no such menu in full version (not dev. preview). is there ...

khorght by Associate II
  • 1562 Views
  • 2 replies
  • 0 kudos

Using J-Link w/Discovery Boards for both F4 and F0 MCUs

Posted on November 12, 2012 at 18:47Greetings - Seek the higher performance (faster downloads) achievable w/J-Link ''SWD'' rather than the ''on-board'' ST-Link.  Reviewed the F4 Discovery schematic - does not appear that there is any easy way to ''b...

jj2 by Associate II
  • 3105 Views
  • 6 replies
  • 0 kudos

EXTI LINE?

Posted on November 12, 2012 at 18:41 I want to edit and use the example of EXTI PA3, but it does not work, what am I doing wrong? void Exti_Config(void) { EXTI_InitTypeDef EXTI_InitStructure; GPIO_InitTypeDef GPIO_InitStructure; N...

orn by Associate II
  • 2191 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.