STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

i2c using std periph library

Posted on February 13, 2012 at 18:12Hi. Anyone has a complete example of use of the i2c protocol (in master and slave mode) for the STM32F4 using the std periph library? the examples included in the library are very confusing, I want an example for ...

FLASH use in STM32F207

Posted on December 19, 2012 at 15:24I want to use the FLASH to write some data for use after power up.1. Is there a small section I can use for some bytes (4) without involve with the CODE flash?2. If not how can I take 1 section of the flash and be...

Barbie by Associate II
  • 1614 Views
  • 4 replies
  • 0 kudos

Question about continuous sampling of multiple ADC channels

Posted on October 01, 2012 at 21:54I would like to continuously sample multiple (~5) channels, preferably with no CPU triggering after the initial setup.  I had been thinking that we would just set up a continuous regular group and then pass back po...

sjenyart by Associate II
  • 5982 Views
  • 13 replies
  • 0 kudos

drive the motor using STM32fr07vg

Posted on December 20, 2012 at 13:37Hi,   i am trying to drive the motor using stm32f407vg. So i use the example code for this project from :\STM32F4xx_DSP_StdPeriph_Lib_V1.0.1\Project\STM32F4xx_StdPeriph_Examples\TIM\6Steps.i changed the code littl...

vinothraj by Associate II
  • 1614 Views
  • 3 replies
  • 0 kudos

Virtual Com Port Driver for WinCE

Posted on December 20, 2012 at 08:51I'm plaing to communicate between STM32F207 and WinCE by VCP(Virtual Com Port). So I need the VCP Driver for WinCE. Does anyone have a good idea to solve this problem?

twoaten by Associate II
  • 679 Views
  • 0 replies
  • 0 kudos

Interrupted CAN ID

Posted on December 17, 2012 at 11:38Hi, Can anybody help me to set up(source code C) CAN id interrupt for STM32F10XX CPU. BR Willy

willy by Associate
  • 1739 Views
  • 3 replies
  • 0 kudos

CAN

Posted on September 19, 2008 at 04:35CAN

steve3 by Associate II
  • 3975 Views
  • 8 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.