STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Timer1 capture data

Posted on December 22, 2012 at 02:07Hi alli run timer 1 in capture mode and i want to know how can i reset the counter.for example i capturing signal and store it  in an array. The counter counting from 0 to 65535 and every time edge comes in interr...

imanpakii by Associate III
  • 2297 Views
  • 4 replies
  • 0 kudos

STM32F050F Flashloader Files for IAR

Posted on November 21, 2012 at 19:36Does anyone have the flashloader files for IAR?  These are the files. *.board *.flash *.mac *.out I can figure out how to modify *.board file from others, but the others are not easy.

jwang by Associate II
  • 2154 Views
  • 5 replies
  • 0 kudos

RTOS

Posted on December 21, 2012 at 15:33 #define IS_SPI_ALL_PERIPH(PERIPH) (((PERIPH) == SPI1) || \ ((PERIPH) == SPI2) || \ ((PERIPH) == SPI3)) #define IS_SPI_ALL_PERIPH(PERIPH) (((PERIPH) == SPI1) || \ ((PERIPH) == SPI2) || \ ((PERIPH) == SPI3...

tinymanta by Associate II
  • 1234 Views
  • 3 replies
  • 0 kudos

STM32F4 tip: reset the cache

Posted on December 09, 2012 at 03:10I had a head-slap moment a few days ago. I eliminated much of the ''quirky behavior'' of my STM32F4Discovery board by having SystemInit() disable and reset the cache. The STM32F4Discovery was my first ST-Link prod...

hfs99 by Associate II
  • 1528 Views
  • 1 replies
  • 0 kudos

STM32F051R8 missing interrupt response

Posted on December 16, 2012 at 14:20During programming trials on a STM32F051 discovery cardlet I found out that the TIM1 update interrupt does not work while using TIM1 channel 4 for PWM input signal evaluation. The update flag UIF is set, but no in...

rfrech by Associate II
  • 1440 Views
  • 3 replies
  • 0 kudos

STM32l152 USART configuration

Posted on December 19, 2012 at 12:47 Hello pals i am new to the stm32 programming, i am trying to configure usart via irq handler, can someone help? #include <stm32l1xx.h> #include ''stm32l1xx_usart.h'' #include ''STM32_Init.h'' void ...

vedhas by Associate II
  • 2957 Views
  • 6 replies
  • 0 kudos

Microseconds delay assembler inline routine IAR EWARM 6.3

Posted on December 19, 2012 at 07:19 I needprecise microseconds delay routine in myapplication ( uses STM32F103RE) I saw https://github.com/leaflabs/libmaple/blob/master/libmaple/include/libmaple/delay.hfor microseconds delay routine. It h...

harinath by Associate III
  • 2553 Views
  • 6 replies
  • 0 kudos

use comparator in Cycle-by-cycle current control loop

Posted on December 19, 2012 at 15:08Hi all, In comparator section of reference manual of stm32f30x devices. It is mentioned: ''Cycle-by-cycle current control loop when combined with the DAC and a PWM output from a timer''. What does it mean? Is th...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.