STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Read Out Protect - Only a section?

Posted on January 31, 2013 at 13:48Hi all,Is it possible to read out protect only one specific area of flash?I want to use a bootloader that can program both encrypted and un-encrypted programs.I need to protect the bootloader from being read so un-...

mwp by Senior
  • 1574 Views
  • 3 replies
  • 0 kudos

Read out Start-Up RAM values

Posted on October 12, 2012 at 11:28Hey there, I am pretty new to micrcontrollers and such. I recently bought a STM32VL Discovery, which I am programming with CoCoox IDE. My goal is to read out the start-up values of internal RAM. By start-up values ...

an by Associate II
  • 10239 Views
  • 27 replies
  • 0 kudos

DAC output not working

Posted on September 05, 2012 at 04:38Hi All, I had the DAC working using DMA to out put a sinewave continuously and it seems to have stopped working when I tried to change which timer I triggered off. After changing the timer configuration back it s...

Dual Quadrature encoders

Posted on January 31, 2013 at 08:04I am trying to read a paid of quadrature encoders, I have managed to get one to read using code copied from this forum but I have been un able to read the second one, I have tried it on different timers (1,3,4) and...

pisaacs9 by Associate II
  • 1292 Views
  • 1 replies
  • 0 kudos

Building 0s/03 doubles timer speed?

Posted on January 24, 2013 at 14:48Hi all,My TIM3 timer is setup to run at 10Khz which it does when i compile with -O0.When i compile with -03 or -Os, the timer speed increases to 20khz.All other build configs (gcc, linker, libs, etc) stay the same....

mwp by Senior
  • 2779 Views
  • 7 replies
  • 0 kudos

Adding RAM and FLASH to STM32F4DISCOVERY board

Posted on January 30, 2013 at 23:01Hi all,I'd like to try uClinux on STM32F4, and I really like STM32F4DISCOVERY. I have two questions :1) Would it be possible to add an external RAM and FLASH chips somehow to this boar, via some free pads / ports t...

drasko by Associate
  • 1638 Views
  • 2 replies
  • 0 kudos

SPI Problem

Posted on January 30, 2013 at 15:02 I am relatively new to the STM32 series. My project has a custom board with a STM32F102C6. I have 2 boards. My first board I have been developing on and everything is working fine. On the 2nd board, the progra...

Problems with Keil and F3 discovery

Posted on December 04, 2012 at 13:08Has anyone else got the F3 discovery working with Keil uVision? The code compiles but when starting a debug session it doesn't seem to deploy and it displays all zeros for the code on the device.I'm using the late...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.