2013-01-31 4:48 AM
Hi all,
Is it possible to read out protect only one specific area of flash?I want to use a bootloader that can program both encrypted and un-encrypted programs.I need to protect the bootloader from being read so un-encrypted (non-trusted) programs cannot access the encryption method/keys in the bootloader.Is this possible somehow?Thanks in advance!2013-01-31 5:53 AM
Ok... so obviously ROP is of no use here as non-trusted firmware can still access the bootloader even if ROP could only be enabled for that section of flash.
So... is there any other way of doing what im after?2013-01-31 6:52 AM
Code running in FLASH, and copied out of flash into RAM, can read the entire memory space.
You could copy data to RAM from a ROP'd device and then reset with BOOTx pins set to execute from RAM, such code would not be able to read the ROM or FLASH.2013-01-31 7:04 AM
Hardware is in production, so i guess it cant be done.
Thanks.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.